Kernel module qca9377 failed to build in latest gatesgarth Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel module qca9377 failed to build in latest gatesgarth Yocto

3,928 Views
brosandic
Contributor II

Hi,

I was using imx-linux-zeus Yocto release ( -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml ) and configuration file with following additional options included to enable qca9377 chip to work on imx7ULP EVK:

MACHINE_FEATURES += " qca9377"
IMAGE_INSTALL_append += " kernel-module-qca9377"
 

With this change, everythin worked fine and I was able to use wifi on the EVK.

However when I tried to switch to the latest Yocto release ( -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0),

build for kernel-module-qca9377 is failing. As far as I can see, this module doesn't have support for kernel 5.10? Can you confirm? Is there a patch available for the qca9377  support in latest imx-linux-gatesgarth?

I have checked available branches on https://source.codeaurora.org/external/imx/qcacld-2.0-imx/ and as far as I could see, there's no support for qca9377 in kernel 5.10? 

Can you please provide a patch so that kernel-module-qca9377 module builds with latest  imx-linux-gatesgarth?

Thanks,

Bogdan

Labels (1)
0 Kudos
Reply
6 Replies

3,074 Views
raajeshk88
Contributor III

@Zhiming_Liu anything on this yet?

3,911 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

I am making this patch.The kernel 5.10.9 has lots of api difference .

BR

Zhiming

0 Kudos
Reply

3,903 Views
brosandic
Contributor II

Hi Zhiming,

Thanks!

When do you think you might have the first working version? 

Is it a matter of days. weeks or months?

Best regards,

Bogdan

0 Kudos
Reply

3,897 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

I recommand you use the L5.4.70_2.3.0,We are gradually replacing with the new wireless in new bsp.

Maybe i need a weeks,a  large number of interfaces have been discarded and the wifi driver cannot use these old interfaces in Kernel 5.10.9 

3,672 Views
asecondi
Contributor I

Hi,

do you have any news about this point?

 

BR,

0 Kudos
Reply

3,895 Views
brosandic
Contributor II

Got it, thank you!

0 Kudos
Reply