Kernel configurations for imx6 sabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel configurations for imx6 sabresd

1,581 次查看
mrigendra_chaub
Contributor III

I have a imx6 sabresd device with 

Processor
i.MX 6Quad* processor
*can be configured as i.MX 6Dual processor

Memory
1 GB DDR3 SDRAM
8 GB eMMC Flash

So device have only 1 gb of DRAM. Then why these configurations are given in imx_v7_android_defconfig

CONFIG_HIGHMEM=y

If the device itself have less memory than 4 gb then why we need it for sabresd?

If I disable this config_highmem I get this log

Truncating RAM at 0x10000000-0x50000000 to -0x47800000
Consider using a HIGHMEM enabled kernel.

from kconfig

The address space of ARM processors is only 4 Gigabytes large and it has to accommodate user address space, kernel address space as well as some memory mapped IO. That means that, if you have a large amount of physical memory and/or IO, not all of the memory can be "permanently mapped" by the kernel. The physical memory that is not permanently mapped is called "high memory".

Depending on the selected kernel/user memory split, minimum vmalloc space and actual amount of RAM, you may not need this option which should result in a slightly faster kernel.

If unsure, say n.

What does it mean? In what way we need this config option. From this thread

HIGHMEMORY in LINUX 

I gather that we don't need it.

Also about initrd (is it initramfs or ramdisk), on extracting contents of boot.img I see below files,

boot-imx6qp.img-base

boot-imx6qp.img-cmdline

boot-imx6qp.img-pagesize

boot-imx6qp.img-ramdisk.gz

boot-imx6qp.img-zImage

here it looks like its a traditional ramdisk not initramfs. But the terminology between ramdisk and initramfs is mixed. Can anyone point me in the correct direction as what nxp source code means about ramdisk and initramfs.

CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE=""

CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_BLK_DEV_RAM_SIZE=8192

标签 (3)
标记 (2)
0 项奖励
回复
1 回复

1,367 次查看
b36401
NXP Employee
NXP Employee

No. The option "CONFIG_HIGHMEM=y" does not not allow to use over 4GB address space.

0 项奖励
回复