Hi all
I want to know the kernel configuration setting of zImage_mfgtool.
How can I know it ?
I used the MFGTool to write a image to eMMC.
When I use the our custom kernel, it failed to write.
On the other hand, when I use the zImage_mfgtool, it success.
So I want to compare the kernel to know the difference between them.
Ko-hey
解決済! 解決策の投稿を見る。
Hello,
From section 6.2 (Manufacturing Tool, MFGTool) of “i.MX_Yocto_Project_User's_Guide.pdf”
A manufacturing tool kernel is built using the imx_v7_mfg_defconfig
while the default kernel is built by using the imx_v7_defconfig.
(/arch/arm/configs/imx_v7_mfg_defconfig)
Since the mfg recipe uses default configuration file to build u-boot and kernel - adaptation of default kernel and U-boot configurations may be needed.
In krogoth release there are sometimes task hask mismatch errors.
A fix for this is to build linux-imx first then clean the linux-mfgtools then bitbake the fsl-image-mfgtool-initramfs.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
From section 6.2 (Manufacturing Tool, MFGTool) of “i.MX_Yocto_Project_User's_Guide.pdf”
A manufacturing tool kernel is built using the imx_v7_mfg_defconfig
while the default kernel is built by using the imx_v7_defconfig.
(/arch/arm/configs/imx_v7_mfg_defconfig)
Since the mfg recipe uses default configuration file to build u-boot and kernel - adaptation of default kernel and U-boot configurations may be needed.
In krogoth release there are sometimes task hask mismatch errors.
A fix for this is to build linux-imx first then clean the linux-mfgtools then bitbake the fsl-image-mfgtool-initramfs.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------