Kernel build fail imx233/stmp3780 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel build fail imx233/stmp3780 board

2,377 次查看
Ameeca
Contributor II

Hi all

 

Im using "./ltib --config" for Freescale iM233/stemp3780.

 

I receive the following error:

 

..snip..
dbus-launch.c: In function 'main':
dbus-launch.c:472: error: impossible constraint in 'asm'
dbus-launch.c:473: error: impossible constraint in 'asm'
make[2]: *** [dbus-launch.o] Error 1
make[2]: Leaving directory `/home/david/Freescale/installed/ltib/rpm/BUILD/dbus-1.2.3/tools'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/david/Freescale/installed/ltib/rpm/BUILD/dbus-1.2.3'
make: *** [all] Error 2
error: Bad exit status from /home/david/Freescale/installed/ltib/tmp/rpm-tmp.37867 (%build)


RPM build errors:
    Bad exit status from /home/david/Freescale/installed/ltib/tmp/rpm-tmp.37867 (%build)
Build time for dbus: 27 seconds

Failed building dbus


f_buildrpms() returned an error, exiting
traceback:
 main:560


Started: Thu Oct  6 14:28:58 2011
Ended:   Thu Oct  6 14:31:52 2011
Elapsed: 174 seconds

These packages failed to build:
dbus

Build Failed

Exiting on error or interrupt

 

I've heard this is either an issue with the dbus make file, I need to uncomment "--without-x", or my "system header files" are buggy. Being totally new to Linux and Linux for embedded systems, I have no idea what this means or how to approach this.

 

Any help would be appreciated.

 

Thanks

标记 (1)
0 项奖励
回复
6 回复数

2,071 次查看
ChaimA
Contributor I

OK

0 项奖励
回复

2,071 次查看
MarioMedinaArza
Contributor I

Thanks for your advice! i had an issue creating ltib for iMX53 START board showing the same error

dbus failed

After adding "-without-x" option to the dist/lfs-5.1/dbus/dbus.spec file, compilation succeeded.

thanks!!

0 项奖励
回复

2,071 次查看
RandyKrakora
NXP Employee
NXP Employee

I found that the dist/lfs-5.1/dbus/dbus.spec file for the 10.07 BSP and the 11.05/09 BSPs were different. If I add the “–without-x” to the configure step in the dbus.spec file in 11.05 it works fine.

 

%Build

export ac_cv_have_abstract_sockets=yes

./configure --prefix=%{_prefix} --host=$CFGHOST --build=%{_build} \

--enable-abstract-sockets --disable-xml-docs --disable-doxygen-docs -without-x

perl -pi -e 's,^sys_lib_search_path_spec=.*,sys_lib_search_path_spec=,' libtool

make

 

 

0 项奖励
回复

2,071 次查看
RandyKrakora
NXP Employee
NXP Employee

So far I've not found anything. I completely removed and re-installed ltib and all the supporting packages and still get the same failure. I'm working with 11.05 and 11.09. I also work with 10.07 and that builds dbus without issues ( in a different VM though ).

0 项奖励
回复

2,071 次查看
RandyKrakora
NXP Employee
NXP Employee

I've been building fine with ltib  for months, then all of a sudden ( I'm sure it's something I've done and cannot pinpoint at the monent ), I got this same error. Building for imx53 QSB ( loco ). I've been working on it on and off today with no resolution yet. If I find something I'll let you know.

0 项奖励
回复

2,071 次查看
Ameeca
Contributor II
bump
0 项奖励
回复