Kernel Panik (oops) on i.mx6s and i.mx6q after activating Closed Security

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Panik (oops) on i.mx6s and i.mx6q after activating Closed Security

3,920 Views
bernhardstrasse
Contributor I

Hi,

in Open Security configuration, Kernel and CAAM runns well, no HAB events. CAAM is build in Kernel.

After activating Closed Security Kernel gets a Kernel Panic (oops).

[6.625359] caam caam.0: failed to instantiate RNG
[6.630163] Unable to handle kernel NULL pointer dereference at virtual address 00000038
[6.638267] pgd = 80004000
[6.640975] [00000038] *pgd=00000000
[6.644568] Internal error: Oops: 5 [#1] PREEMPT

if i compile kernel with CAAM as modul settings the Kernel starts, building CAAM Kernel Module not work

Kernel build log : (CAAM as Module Configuration)

  LD  arch/arm/boot/compressed/vmlinux

  OBJCOPY arch/arm/boot/zImage

  Kernel: arch/arm/boot/zImage is ready

  Building modules, stage 2.

  MODPOST 7 modules

ERROR: "caam_algapi_hash_startup" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_algapi_shutdown" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_sm_startup" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_sm_shutdown" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_rng_shutdown" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_algapi_hash_shutdown" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_algapi_startup" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_sm_example_init" [drivers/crypto/caam/caam.ko] undefined!

ERROR: "caam_rng_startup" [drivers/crypto/caam/caam.ko] undefined!

make[1]: *** [__modpost] Error 1

make: *** [modules] Error 2

Board: Custom Board ->based on Sabrelite Board

CPU: i.MX6s i.MX6q (separate kernel config)

Kernel 3.0.35 (BSP4.0.0)

who knows this trouble? there solutions?


regards Bernhard

Boot Log: (CAAM build in Kernel Configuration) after Security Closed

[ 3.923219] mmc0: no vmmc regulator found
[ 3.929440] mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using ADMA
[ 3.936662] sdhci sdhci-esdhc-imx.0: no card-detect pin available!
[ 3.943864] mmc1: no vmmc regulator found
[ 3.954129] mmc1: SDHCI controller on platform [sdhci-esdhc-imx.0] using ADMA
[ 4.052546] mmc0: new SDIO card at address 0001
[ 4.204879] mmc1: new SDIO card at address 0001
[ 6.625359] caam caam.0: failed to instantiate RNG
[ 6.630163] Unable to handle kernel NULL pointer dereference at virtual address 00000038
[ 6.638267] pgd = 80004000
[ 6.640975] [00000038] *pgd=00000000
[ 6.644568] Internal error: Oops: 5 [#1] PREEMPT
[ 6.649188] Modules linked in:
[ 6.652258] CPU: 0 Not tainted  (3.0.35-2039-g267e004-svn5792 #13)
[ 6.658716] PC is at caam_sm_shutdown+0x18/0x2c
[ 6.663249] LR is at caam_sm_shutdown+0x14/0x2c
[ 6.667782] pc : [<802fbac0>]lr : [<802fbabc>]psr: 60000013
[ 6.667787] sp : 8d007eb0  ip : 00000001  fp : 804c4060
[ 6.679273] r10: 804c4060  r9 : 8f8e0000  r8 : fffffffb
[ 6.684500] r7 : 8f8e0000  r6 : 8e020800  r5 : 8cc2d540  r4 : 00000000
[ 6.691030] r3 : 802f1e10  r2 : 88003000  r1 : 8b900060  r0 : 00000000
[ 6.697562] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel
[ 6.704874] Control: 10c53c7d  Table: 10004059  DAC: 00000015
[ 6.710622] Process swapper (pid: 1, stack limit = 0x8d0062e8)
[ 6.716459] Stack: (0x8d007eb0 to 0x8d008000)
[ 6.720819] 7ea0: 8e020800 802f150c 802f1e10 8cc2d540
[ 6.729002] 7ec0: ffffffed 8e020800 8f8e0000 802f1e74 00000000 00000001 8c022390 8e020808
[ 6.737184] 7ee0: 8e029600 33000000 8e020808 8e020808 80511970 8e02083c 00000000 804f02bc
[ 6.745366] 7f00: 00000000 800218cc 00000000 8024096c 80240954 8023f748 8e020808 804f02bc
[ 6.753548] 7f20: 8e02083c 00000000 00000000 8023f8e0 804f02bc 00000000 8023f854 8023e968
[ 6.761729] 7f40: 8d8010f8 8e003450 804f02bc 804ea2a8 8c872480 8023f11c 8047b074 801ed36c
[ 6.769911] 7f60: 804f02bc 804f02bc 8d006000 800355e0 00000000 00000000 800218cc 8023fdb4
[ 6.778092] 7f80: 804f9580 8d006000 800355e0 00000000 00000000 8002f34c 00000000 8d81b4e0
[ 6.786274] 7fa0: 800951c8 800218cc 804dd3f8 800951f8 000001df 800355e0 00000013 37340000
[ 6.794456] 7fc0: 00000039 80027bc8 80027c38 800355e0 00000013 00000000 00000000 00000000
[ 6.802638] 7fe0: 00000000 800089e8 00000000 00000000 80008964 800355e0 ebffeffb eaeeffdf
[ 6.810831] [<802fbac0>] (caam_sm_shutdown+0x18/0x2c) from [<802f150c>] (caam_remove+0x20/0xc4)
[ 6.819539] [<802f150c>] (caam_remove+0x20/0xc4) from [<802f1e74>] (caam_probe+0x8c4/0xa70)
[ 6.827902] [<802f1e74>] (caam_probe+0x8c4/0xa70) from [<8024096c>] (platform_drv_probe+0x18/0x1c)
[ 6.836881] [<8024096c>] (platform_drv_probe+0x18/0x1c) from [<8023f748>] (driver_probe_device+0x90/0x19c)
[ 6.846546] [<8023f748>] (driver_probe_device+0x90/0x19c) from [<8023f8e0>] (__driver_attach+0x8c/0x90)
[ 6.855948] [<8023f8e0>] (__driver_attach+0x8c/0x90) from [<8023e968>] (bus_for_each_dev+0x5c/0x88)
[ 6.865003] [<8023e968>] (bus_for_each_dev+0x5c/0x88) from [<8023f11c>] (bus_add_driver+0x17c/0x244)
[ 6.874145] [<8023f11c>] (bus_add_driver+0x17c/0x244) from [<8023fdb4>] (driver_register+0x78/0x13c)
[ 6.883290] [<8023fdb4>] (driver_register+0x78/0x13c) from [<8002f34c>] (do_one_initcall+0x34/0x174)
[ 6.892437] [<8002f34c>] (do_one_initcall+0x34/0x174) from [<800089e8>] (kernel_init+0x84/0x124)
[ 6.901237] [<800089e8>] (kernel_init+0x84/0x124) from [<800355e0>] (kernel_thread_exit+0x0/0x8)
[ 6.910031] Code: ebfd0dfb e5900060 ebfd0df9 e1a04000 (e5900038)
[ 6.916157] ---[ end trace f74bc9c599f351aa ]---
[ 6.920785] Kernel panic - not syncing: Attempted to kill init!
[ 6.926736] [<80039a2c>] (unwind_backtrace+0x0/0xf8) from [<803a0040>] (panic+0x64/0x178)
[ 6.934940] [<803a0040>] (panic+0x64/0x178) from [<80063018>] (do_exit+0x670/0x6f8)
[ 6.942607] [<80063018>] (do_exit+0x670/0x6f8) from [<80038198>] (die+0x22c/0x2a0)
[ 6.950197] [<80038198>] (die+0x22c/0x2a0) from [<8039fa24>] (__do_kernel_fault.part.5+0x54/0x74)
[ 6.959092] [<8039fa24>] (__do_kernel_fault.part.5+0x54/0x74) from [<8003d5f0>] (do_page_fault+0x2b4/0x31c)
[ 6.968853] [<8003d5f0>] (do_page_fault+0x2b4/0x31c) from [<8002f194>] (do_DataAbort+0x34/0x9c)
[ 6.977569] [<8002f194>] (do_DataAbort+0x34/0x9c) from [<80034710>] (__dabt_svc+0x70/0xa0)
[ 6.985842] Exception stack(0x8d007e68 to 0x8d007eb0)
[ 6.990901] 7e60: 00000000 8b900060 88003000 802f1e10 00000000 8cc2d540
[ 6.999093] 7e80: 8e020800 8f8e0000 fffffffb 8f8e0000 804c4060 804c4060 00000001 8d007eb0
[ 7.007281] 7ea0: 802fbabc 802fbac0 60000013 ffffffff
[ 7.012346] [<80034710>] (__dabt_svc+0x70/0xa0) from [<802fbac0>] (caam_sm_shutdown+0x18/0x2c)
[ 7.020975] [<802fbac0>] (caam_sm_shutdown+0x18/0x2c) from [<802f150c>] (caam_remove+0x20/0xc4)
[ 7.029692] [<802f150c>] (caam_remove+0x20/0xc4) from [<802f1e74>] (caam_probe+0x8c4/0xa70)
[ 7.038060] [<802f1e74>] (caam_probe+0x8c4/0xa70) from [<8024096c>] (platform_drv_probe+0x18/0x1c)
[ 7.047038] [<8024096c>] (platform_drv_probe+0x18/0x1c) from [<8023f748>] (driver_probe_device+0x90/0x19c)
[ 7.056711] [<8023f748>] (driver_probe_device+0x90/0x19c) from [<8023f8e0>] (__driver_attach+0x8c/0x90)
[ 7.066121] [<8023f8e0>] (__driver_attach+0x8c/0x90) from [<8023e968>] (bus_for_each_dev+0x5c/0x88)
[ 7.075184] [<8023e968>] (bus_for_each_dev+0x5c/0x88) from [<8023f11c>] (bus_add_driver+0x17c/0x244)
[ 7.084325] [<8023f11c>] (bus_add_driver+0x17c/0x244) from [<8023fdb4>] (driver_register+0x78/0x13c)
[ 7.093474] [<8023fdb4>] (driver_register+0x78/0x13c) from [<8002f34c>] (do_one_initcall+0x34/0x174)
[ 7.102622] [<8002f34c>] (do_one_initcall+0x34/0x174) from [<800089e8>] (kernel_init+0x84/0x124)
[ 7.111424] [<800089e8>] (kernel_init+0x84/0x124) from [<800355e0>] (kernel_thread_exit+0x0/0x8)

Labels (3)
0 Kudos
11 Replies

1,530 Views
ottob
Contributor IV

We are using the Yocto release from May and are seeing the same (seemingly common) problem.

Please advice,

/Otto

----

platform 2101000.jr0: 2000025b: CCB: desc idx 2: RNG: Hardware error.

platform 2101000.jr0: unable to instantiate RNG

Unable to handle kernel NULL pointer dereference at virtual address 00000034

pgd = 80004000

[00000034] *pgd=00000000

Internal error: Oops: 5 [#1] PREEMPT SMP ARM

Modules linked in:

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.10.17-1.0.0_ga+g232293e #70

task: a805c000 ti: a805a000 task.ti: a805a000

PC is at caam_algapi_init+0x6c/0x4dc

LR is at caam_algapi_init+0x64/0x4dc

pc : [<80bff968>]    lr : [<80bff960>]    psr: a0000113

sp : a805beb8  ip : 80632dc0  fp : 00000000

r10: 00000000  r9 : a815b210  r8 : 80c6c840

r7 : 80c6c840  r6 : 80c6c840  r5 : 00000006  r4 : 80c17400

r3 : 00000000  r2 : a805be88  r1 : 000000d0  r0 : 00000000

0 Kudos

1,530 Views
george
Senior Contributor II

Dear Otto,

We have solved it.

However, I do not remember it in detail now.

The kernel version which we used was 3.0.35.

Maybe 6400 was set to RNG4_ENT_CLOCKS_SAMPLE.

RNG4_ENT_CLOCKS_SAMPLE is defined in intern.h.

If I become free, it will inform a little in more detail.

BR,

George

0 Kudos

1,530 Views
ottob
Contributor IV

George,

For now we decided to simply turn off the CAAM functions as they are not that important for our project.

Thanks for your help and have a great weekend !

/Otto

0 Kudos

1,530 Views
Yuri
NXP Employee
NXP Employee
0 Kudos

1,530 Views
george
Senior Contributor II

Dear Yuri,

I need your help.

A phenomenon similar also to my customer's board occurs.

boot.log (Attached file)

.

platform caam_jr.0: 2000025b: CCB: desc idx 2: RNG: Hardware error.
platform caam_jr.0: unable to instantiate RNG
Unable to handle kernel NULL pointer dereference at virtual address 00000038

.

.

Kernel panic - not syncing: Attempted to kill init!

It seems to me that following patch file can improve this phenomenon.

ENGR00290444: Need to update CAAM driver with SM patches from STC

Since we are using L3.0.35_4.1.0_ER_SOURCE_BSP, it does not include the patch.

Is my understanding correct?

Best Regards,

George

0 Kudos

1,530 Views
Yuri
NXP Employee
NXP Employee

If You are using BSP release 3.0.35_4.1.0 :

there are fixes for CAAM driver and black keys test application, the

patches are not part of the formal BSP and are online in our git repository:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.1.0

Patches related to CAAM changes are:

ENGR00290444: Need to update CAAM driver with SM patches from STC

ENGR00290448: Double instantiation of RNG in CAAM Driver

ENGR00290449: Cannot build CAAM as a loadable module

ENGR00291081 CAAM: Fix the Copyright issue introduced by commit: 2b94a4b

0 Kudos

1,530 Views
satoshishimoda
Senior Contributor I

Dear Yuri,

Our customer have a very similar issue.

So could you give us a advice how avoid RNG hardware error?

Best Regards,

Satoshi Shimoda

0 Kudos

1,530 Views
george
Senior Contributor II

Dear Yuri,

Thank you for your response.

We had already found and applied those patches.

And kernel-panic was avoidable.

However, the RNG Hardware error occurs rarely.

  platform caam_jr.0: 2000025b: CCB: desc idx 2: RNG: Hardware error.

  platform caam_jr.0: unable to instantiate RNG

  caam caam.0: error instantiating rng, terminating

We are looking for workaround.

For example, CAAM initialization is repeated until it is successful.

If there is some advice, please let me know.

Best Regards,

George

0 Kudos

1,530 Views
Yuri
NXP Employee
NXP Employee

With regards to the RNG failure, please have the customer add the below

lines to their .csf file after the [Authenticate CSF] section.

[Unlock]

Engine = CAAM

Features = RNG

It should be done fo both U-Boot and UImage ".csf" files.

~Yuri.

0 Kudos

1,530 Views
george
Senior Contributor II

Dear all,

kernle - .config file is attached.

BR,

George

0 Kudos

1,530 Views
georgebonser
Contributor I

I am having exactly the same problem.  When I click the link you provided in your reply, I get an "Unauthorized" banner.  Basically I see no indication that CAAM is initializing when it is compiled in. When I attempt to compile it as a module I get the same "undefined" errors as described by the original poster.

George

0 Kudos