Trying to Bring up Kernel from Git repo.
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.14.28_1.0.0_ga
Kernel Panic is observed in imx6_pm_common_init
[ 0.066166] Unable to handle kernel paging request at virtual address f4000000
[ 0.073495] pgd = 80004000
[ 0.076297] [f4000000] *pgd=00000000
[ 0.079982] Internal error: Oops - BUG: 805 [#1] ARM
[ 0.085045] Modules linked in:
[ 0.088212] CPU: 0 PID: 1 Comm: swapper Not tainted 3.14.28 #40
[ 0.094235] task: 8c058000 ti: 8c05c000 task.ti: 8c05c000
[ 0.099746] PC is at imx6_pm_common_init+0x70/0x26c
[ 0.104728] LR is at suspend_set_ops+0x90/0xa0
[ 0.109272] pc : [<805666cc>] lr : [<8005b038>] psr: 60000153
[ 0.109272] sp : 8c05de80 ip : 8c05de68 fp : 8c05de9c
[ 0.120949] r10: 8058d3d8 r9 : 00000000 r8 : 805567e8
[ 0.126273] r7 : 805f1d40 r6 : 805a18d0 r5 : 8058d3c0 r4 : f4000000
[ 0.132902] r3 : 00000000 r2 : f4000000 r1 : 00000000 r0 : 805f2edc
[ 0.139533] Flags: nZCv IRQs on FIQs off Mode SVC_32 ISA ARM Segment kernel
[ 0.147032] Control: 10c53c7d Table: 10004059 DAC: 00000015
[ 0.152878] Process swapper (pid: 1, stack limit = 0x8c05c230)
[ 0.158811] Stack: (0x8c05de80 to 0x8c05e000)
[ 0.163273] de80: 8c14cc00 8058d3c0 805a4360 805f1d40 8c05deac 8c05dea0 80566a80 80566668
[ 0.171560] dea0: 8c05dec4 8c05deb0 8055f7ac 80566a78 8058c464 00000003 8c05ded4 8c05dec8
[ 0.179849] dec0: 8055680c 8055f5bc 8c05df54 8c05ded8 80008818 805567f4 8c05df04 80044214
[ 0.188138] dee0: 8fffc2ab 8fffc2a5 8c05df00 8c05def8 80044214 80044198 8fffc2a5 00000000
[ 0.196426] df00: 8c05df54 8c05df10 80044400 805554d8 00000000 8055372c 00000003 00000003
[ 0.204714] df20: 00000061 8055311c 8c05df54 00000003 8058d3c0 805a4360 805f1d40 00000061
[ 0.213002] df40: 00000000 8058d3d8 8c05df94 8c05df58 80555b48 80008780 00000003 00000003
[ 0.221289] df60: 805554cc 00000000 00000000 00000000 00000000 803e05b0 00000000 00000000
[ 0.229577] df80: 00000000 00000000 8c05dfac 8c05df98 803e05c8 80555a64 8c05c000 00000000
[ 0.237864] dfa0: 00000000 8c05dfb0 8000e378 803e05bc 00000000 00000000 00000000 00000000
[ 0.246151] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.254438] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[ 0.262718] Backtrace:
[ 0.265278] [<8056665c>] (imx6_pm_common_init) from [<80566a80>] (imx6dl_pm_init+0x14/0x1c)
[ 0.273734] r7:805f1d40 r6:805a4360 r5:8058d3c0 r4:8c14cc00
[ 0.279542] [<80566a6c>] (imx6dl_pm_init) from [<8055f7ac>] (imx6q_init_machine+0x1fc/0x27c)
[ 0.288093] [<8055f5b0>] (imx6q_init_machine) from [<8055680c>] (customize_machine+0x24/0x48)
[ 0.296720] r4:00000003 r3:8058c464
[ 0.300420] [<805567e8>] (customize_machine) from [<80008818>] (do_one_initcall+0xa4/0x118)
[ 0.308884] [<80008774>] (do_one_initcall) from [<80555b48>] (kernel_init_freeable+0xf0/0x1b8)
[ 0.317599] r10:8058d3d8 r9:00000000 r8:00000061 r7:805f1d40 r6:805a4360 r5:8058d3c0
[ 0.325582] r4:00000003
[ 0.328228] [<80555a58>] (kernel_init_freeable) from [<803e05c8>] (kernel_init+0x18/0xf4)
[ 0.336508] r10:00000000 r8:00000000 r7:00000000 r6:00000000 r5:803e05b0 r4:00000000
[ 0.344501] [<803e05b0>] (kernel_init) from [<8000e378>] (ret_from_fork+0x14/0x20)
[ 0.352171] r4:00000000 r3:8c05c000
[ 0.355865] Code: e282233d e0822221 e203140a e0824221 (e7823221)
[ 0.362080] ---[ end trace 994439b5388a6327 ]---
[ 0.366798] Kernel panic - not syncing: Fatal exception
[ 82.909701] random: nonblocking pool is initialized
解決済! 解決策の投稿を見る。
This Problem is solved now.
PM code is completely changed in 3.14.28 kernel.
iram_tlb_base_addr Variable was not getting initialized since it was not able to find DT poperty fsl,lpm-sram which is responsible for IRAM/OCRAM allocation.
Enabled the DT configuration to fix this issue.
This Problem is solved now.
PM code is completely changed in 3.14.28 kernel.
iram_tlb_base_addr Variable was not getting initialized since it was not able to find DT poperty fsl,lpm-sram which is responsible for IRAM/OCRAM allocation.
Enabled the DT configuration to fix this issue.
Hi Dilshad
please try ldo mode (not ldo bypass) and check processor power supplies.
One can check Chapter 4 Requirements for Power Management IMX6DQ6SDLHDG
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for your reply.
Can you please suggest the changes which needs to be incorporated for this?
Regards,
Dilshad
Hi Dilshad
please try with imx6q-sabresd-ldo.dts
Best regards
igor
Hi Igor,
I have tried it, but result is same.
Could you please tell changes incorporated between 3.10.17 and 3.14.28 kernel for mach-imx/pm-imx6.c file.
or
Any application note on Power Domain related changed between these two versions?
Thanks,
Dilshad
Hi Dilshad
for changes you can look at linux documents
L3.10.17_1.0.0_IMX6QDLS_BUNDLE
L3.14.28_1.0.0_iMX6QDLS_BUNDLE
I am not aware of any application notes describing linux power
management drivers. Suggest to build minimal image and try.
What PMIC are you using ? Had you checked power voltages by osilloscope,
are they comply with datasheet requirements ?
Best regards
igor