Kernel 3.14, video issues with supported cea mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kernel 3.14, video issues with supported cea mode

跳至解决方案
2,137 次查看
angelo_d
Senior Contributor I

Dear all,

i have seen that in 3-14 imx6 kernel,  the mode 1280x800 for hdmi (have Adafruit hdmi lcd with this mode) is no more supported. Kernel allows only cea mode 1280x720.

Setting 1280x800M60 in kernel boot params,

Kernel 3.11 was still allowing 1280x800 reso:

[system@localhost ~]$ cat /sys/class/graphics/fb2/mode

U:1280x800p-60

while 3.14 not, so i ged a stretched image in the hdmi display

[user@localhost ~]$ cat /sys/class/graphics/fb2/mode

S:1280x720p-60

If i set 1280x720M60 as kernel params, nothing changes. Every help is appreciated.

Best regards

标签 (2)
0 项奖励
回复
1 解答
2,006 次查看
angelo_d
Senior Contributor I

Hi, found this solution

Re: How to add HDMI resolution to i.MX6 Yocto BSP.

Of course also wxga mode struct need to be added.

Thanks

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,007 次查看
angelo_d
Senior Contributor I

Hi, found this solution

Re: How to add HDMI resolution to i.MX6 Yocto BSP.

Of course also wxga mode struct need to be added.

Thanks

0 项奖励
回复
2,006 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi andelo dureghello,

I am very glad to hear of you have found the way to solve your problem. Welcome to create new threads in our community.

Have a nice day.

Best Regards

Dan

0 项奖励
回复