Karo TX6Q i.MX6Q 1080p FHD WEC7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Karo TX6Q i.MX6Q 1080p FHD WEC7

753件の閲覧回数
fcnewbie
Contributor I

Hello,

I want to use the Karo TX6Q LVDS module http://www.karo-electronics.com/tx6.html

running on WEC7, to display full HD 1920 x 1080 onto a 21.5" LCD with dual LVDS channels. The BSP available does not support 1080 FHD split channel output.

Has anyone managed to configure the LVDS display bridge (LDB), so that the output LVDS ports are used as split channel and had 1080 FHD running please? If so, how?

Thanks

ラベル(1)
0 件の賞賛
返信
0 返答(返信)