KSZ8041 and i.MX6DL with external clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSZ8041 and i.MX6DL with external clock

ソリューションへジャンプ
2,366件の閲覧回数
steffendoster
Contributor IV

Hello everyone,

I have a problem with setting up the common clock for mac and phy of a custom i.MX6-Board:

The phy and the i.MX6 are supplied with a 50MHz clock by an external oscillator.

The connected Pin on i.MX6 is RGMII_TX_CTL.

The Interface between i.MX6 and Phy is "rmii".

Devicetree-Enty for FEC:

fec: ethernet@02188000 {
   compatible = "fsl,imx6q-fec";
   reg = <0x02188000 0x4000>;
   interrupts-extended =
   <&intc 0 118 IRQ_TYPE_LEVEL_HIGH>,
   <&intc 0 119 IRQ_TYPE_LEVEL_HIGH>;
   interrupt-names = "int0", "pps";
   clocks = <&clks IMX6QDL_CLK_ENET>,
   <&clks IMX6QDL_CLK_ENET>,
   <&clks IMX6QDL_CLK_ENET_REF>;
   clock-names = "ipg", "ahb", "enet_out";
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_enet>;
   phy-mode = "rmii";
   ref-clock = <50000000>;
   phy-reset-gpios = <&gpio4 8 GPIO_ACTIVE_LOW>;
   phy-reset-duration = <2>;
   fsl,magic-packet;

   max-speed = <100>; /* Allow only 100MBit */

   status = "okay";
};

Devicetree-Entry for IOMUX:

/* Pinmuxing for the connection to the RMII Phy */
pinctrl_enet: enetgrp {
   fsl,pins = <
   MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0f0
   MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0f0
   MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x1b0f0
   MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x1b0f0
   MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x1b0f0
   MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x1b0f0
   MX6QDL_PAD_RGMII_TX_CTL__ENET_REF_CLK 0x1b0f0
   MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x1b0f0
   MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x1b0f0
   MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x1b0f0
   MX6QDL_PAD_GPIO_17__GPIO7_IO12 0x1b0f0                      /*INTERRUPT*/
   MX6QDL_PAD_KEY_COL1__GPIO4_IO08 0x1b0f0                   /*RESET*/
   >;
};

The Phy works fine with U-Boot, but it seems that the Linux-Kernel sets RGMII_TX_CTL as Output for the Clock.

This results in a weird "clock-collision" which makes an Ethernet Link almost impossible.

I also tried

clock-names = "ipg", "ahb", "ptp";

but with the same result.

What am I doing wrong? How can I set the RGMII_TX_CTL correctly as clock source for the i.MX6?

ラベル(2)
1 解決策
2,051件の閲覧回数
steffendoster
Contributor IV

Well I solved the Problem:

I was not able to convince the Kernel to use the Pin as Input. So I removed the external oscillator and connected the phy directly with the clock pin of i.MX6.

Now it works very smoothly and stable.

The only thing I also had to change was the U-Boot, because the bootloader used this pin as Input and has an option for a netboot.

Now the Bootloader also uses the pin as output and can do a netboot as always.

元の投稿で解決策を見る

5 返答(返信)
2,052件の閲覧回数
steffendoster
Contributor IV

Well I solved the Problem:

I was not able to convince the Kernel to use the Pin as Input. So I removed the external oscillator and connected the phy directly with the clock pin of i.MX6.

Now it works very smoothly and stable.

The only thing I also had to change was the U-Boot, because the bootloader used this pin as Input and has an option for a netboot.

Now the Bootloader also uses the pin as output and can do a netboot as always.

2,051件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Steffen

one can check in probe function of enet driver

ENET_REF_CLK, bit ENET_CLK_SEL in IOMUXC_GPR1 register.

Try with NXP Linux L4.14.98_2.0.0   
linux-imx - i.MX Linux kernel 

Linux L4.14.98_2.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
2,051件の閲覧回数
steffendoster
Contributor IV

Hi Igor,

thanks for your answer, but I forgot to mention, that I already knew, bit 21 in IOMUXC_GPR1 is set.

My Question is more about how to write the devicetree so the kernel unsets the bit.

Or do I have to patch the Kernel?

0 件の賞賛
2,051件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Steffen

available options through device tree are described in documentation

fsl-fec.txt\net\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

If there are no such options one can try to patch.

Best regards
igor

0 件の賞賛
2,051件の閲覧回数
steffendoster
Contributor IV

That was a very nice hint!

The clocks were not correctly documented in my Kernel (4.19.56 Mainline). I changed 

clock-names = "ipg", "ahb", "enet_out";

to 

clock-names = "ipg", "ahb", "enet_clk_ref";

and got a clean 50MHz clock.

But now the signal seems to be too small neither for MAC or PHY. I get the error

fec 2188000.ethernet eth0: Unable to connect to phy

from Kernel.

EDIT:

IOMUXC_GPR1 0x020E0004 = 0x48601005

Bit 21 is still '1'   ????

0 件の賞賛