KNX with i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,812件の閲覧回数
atillametetured
Contributor V

Greetings,

Did anyone here ever implement any KNX solutions using i.MX6 as a host. If so

which transceiver did you use?

Thanks

ラベル(1)
1 解決策
1,603件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Hi Atilla,

on our LPC boards we use chip from OnSemi IC NCN5120. For example AN11231: KNX evaluation board using LPC1227 and NCN5120 | www.LPCware.com It can be replicated on i.MX6.

Michal

元の投稿で解決策を見る

2 返答(返信)
1,604件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Hi Atilla,

on our LPC boards we use chip from OnSemi IC NCN5120. For example AN11231: KNX evaluation board using LPC1227 and NCN5120 | www.LPCware.com It can be replicated on i.MX6.

Michal

1,603件の閲覧回数
atillametetured
Contributor V

Hello Michal,

Thanks for the information.

Mete

0 件の賞賛
返信