Jump Start on Designing a module around i.MX6 Quad Automotive Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Jump Start on Designing a module around i.MX6 Quad Automotive Processor

1,625件の閲覧回数
bharathkumar
Contributor I

Hi Community,

I'm in need of building a custom board (module) using i.MX6 Quad Processor.

I need to Jump start on the design of board, but the firmware booting is the concept unclear for me to proceed.

Can anyone please give some in-detail description on how to make the provision for loading boot code (to port Linux) on to my custom board.

Thanks & Best Regards,

Bharath Kumar Chowdary Gundala

タグ(1)
0 件の賞賛
返信
1 返信

1,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bharath

one can start with i.MX Hardware Design Guide and Board Bring Up presentation

https://community.freescale.com/servlet/JiveServlet/downloadBody/104602-102-1-23487/APF-DES-T1023.pd...

and attached Proting Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信