Hello,
I'm designing a project base on I.mx rt 1050.
I saw the jtag configuration in the EVM, I'll like to create my own jtag connected directly to the i.mx rt instead of using mk20 for that.
Can I use the pinout configuration by segger J-link 9 pin cortex M adapter?
This is the link for the cortex M adapter of seger:
9-Pin Cortex M Adapter | SEGGER - The Embedded Experts
Thanks,
Snir
Hi Snir
yes seems it can be used, RT1050 EVK debug interface is described in
sect.2.12. JTAG Connector MIMXRT1050 EVK Board Hardware User’s Guide
(swd is supported)
https://www.nxp.com/docs/en/user-guide/MIMXRT1050EVKHUG.pdf
jtag usage is described on
MCUXpresso IDE V10.1.0 with i.MX RT1052 Crossover Processor | MCU on Eclipse
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------