Java SE on imx25

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Java SE on imx25

2,594 次查看
erhan14
Contributor I

Hi,

I want to add Java SE support using OpenJDK with Cacao VM to imx258 demo board.

How can I configure ltib to prepare a flash image with Java support?

Thanks

标签 (2)
标记 (3)
0 项奖励
回复
7 回复数

2,282 次查看
OtavioSalvador
Senior Contributor II

If you are open to work in adding i.MX25 support in Yocto Project BSP (see FSL Community BSP) the later Java addition is quite trivial. We have the meta-java that has all this done and provides several Open Source VM alternatives.

Currently the i.MX25 is not supported by the BSP, that's why I put this remark there.

0 项奖励
回复

2,282 次查看
erhan14
Contributor I

Is there a step by step guide for porting the official BSP to Yocto based one?

0 项奖励
回复

2,282 次查看
OtavioSalvador
Senior Contributor II

No; there's no such guide yet.

I can try to help if you want. Otherwise you can hire us (or someone else) to do the work. Either way works.

Initial support using mainline kernel and mainline U-Boot should be trivial. The i.MX25 2.6.31 kernel might be a little bit more problematic (due the fixes need for toolchain compatibility and others) but also doable.

0 项奖励
回复

2,282 次查看
erhan14
Contributor I

Freescale released official Yocto release but I cannot find imx25 port in it?

0 项奖励
回复

2,282 次查看
OtavioSalvador
Senior Contributor II

As I said previously it has not been added.

Someone needs (or sponsor a company) to do it and maintain it.

0 项奖励
回复

2,282 次查看
Yuri
NXP Employee
NXP Employee

Please use the following from Community :

“All Boards Java”

https://community.freescale.com/docs/DOC-1478

Note, for i.MX25 we should use ARMv5 packages :

http://www.oracle.com/technetwork/java/embedded/downloads/javase/index.html

0 项奖励
回复

2,282 次查看
erhan14
Contributor I

Hi,

Thanks for the quick response.

I actually want to use opensource VM alternatives as Oracle Java is licensed for embedded use.

Thanks

0 项奖励
回复