Java ME support in i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Java ME support in i.MX6

跳至解决方案
3,215 次查看
ko-hey
Senior Contributor II

Hi all

I want to know a support of Java ME in i.MX6.

My customer want to use i.MX6UL with Linux and end customer also want to use CLDC 1.1 of Java ME.

Connected Limited Device Configuration (CLDC) is as flow.

Connected Limited Device Configuration (CLDC)

Connected Limited Device Configuration - Wikipedia, the free encyclopedia

I searched a i.MX Community and found following thread. But I couldn't figure out. So please let me know.

All Boards Java

NXP ARM-based processor with Java SE support

Can i.MX6UL support CLDC 1.1 ?

Ko-hey

标签 (4)
0 项奖励
回复
1 解答
2,295 次查看
SergioSolis
NXP Employee
NXP Employee

Yes, you can use Java ME 8 for the i.MX6, please take a look at the following document:

http://www.oracle.com/technetwork/java/embedded/javame/embed-me/documentation/me-e-otn-faq-1852008.p...

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,296 次查看
SergioSolis
NXP Employee
NXP Employee

Yes, you can use Java ME 8 for the i.MX6, please take a look at the following document:

http://www.oracle.com/technetwork/java/embedded/javame/embed-me/documentation/me-e-otn-faq-1852008.p...

0 项奖励
回复
2,295 次查看
janekschumann
Contributor II

This seems to be the only source I could find regarding i.MX6 and Java ME 8.

Can you please clarify your answer:

is Java ME 8 (Embedded) supported on the Cortex-A9 cores out-of-the-box? (like i.MX6 DualLite)

The linked documentation only talks about Cortex-M4 (which would be i.MX6 SoloX) as well as ARM9. As far as I know, ARM9 is not the same as the ARM Cortex-A9 used in the i.MX6, or is it?

Do you have any supporting documentation on how to get Java ME 8 up and running on an (Cortex-A9) i.MX6?

Your help is much appreciated.

Janek

0 项奖励
回复
2,295 次查看
ko-hey
Senior Contributor II

Hi SergioSolis

Thanks!!

0 项奖励
回复