Jailhouse porting onto imx.8mq

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Jailhouse porting onto imx.8mq

575件の閲覧回数
MEGHANAB
Contributor I

For the i.MX 8MQ prebuilt image provided,does it include jailhouse hypervisor,the required kernel modules(jailhouse.ko,uio_ivshmem.ko),and guest os cell configuration.If yes pls provide the link for the prebuilt image
Regards
Meghana

0 件の賞賛
返信
4 返答(返信)

557件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MEGHANAB 

 

I hope you are doing very well.

 

Please refer to the chapter 5.6.11 Building Jailhouse of the i.MX Yocto Project User's Guide.

There is described how to build Jailhouse for i.MX8MQ.

 

Best regards,

Salas.

0 件の賞賛
返信

538件の閲覧回数
MEGHANAB
Contributor I
Please mention which linux bsp is supported for imx8mq jailhouse.
Regards
0 件の賞賛
返信

513件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MEGHANAB 

 

The version that you are using is compatible with Jailhouse Hypervisor.

How did you flashed your image?

 

Best regards,

Salas.

0 件の賞賛
返信

541件の閲覧回数
MEGHANAB
Contributor I

So, Should i have to build the image with yocto instead of using prebuilt one?
But when I'm booting the prebuilt image the board is not getting booted.I have used LF_v6.12.3-1.0.0_images_IMX8MQEVK.Please do the needful.
Thank you

0 件の賞賛
返信