JTAG_MOD settings for i.MX 8M Nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG_MOD settings for i.MX 8M Nano

3,305 Views
peterlischer
Senior Contributor I

According to the reference manual of the i.MX 8M Mini, in order to enable the IEEE1149.1 standard features of the JTAG interface, the TEST_MODE, BOOT_MODE1, BOOT_MODE0, and JTAG_MOD have to be set to 1110. I now saw the exact same note in the reference manual for the i.MX 8M Nano (Rev. 0 12/2019) on page 206. However, this does not make any sense. The i.MX 8M Nano does not have a TEST_MODE pin. On the other hand, the Nano features additionally BOOT_MODE2 and BOOT_MODE3.

How do the pins need to be strapped on the i.MX 8M Nano for enabling the IEEE1149.1 feature?

Labels (1)
Tags (2)
0 Kudos
Reply
8 Replies

2,323 Views
estiven
Contributor I

Hi @weidong_sun,

I have the same issue as the bill_tucker. When i pulling the BOOT_MODE3_0 signals to "1111" to enter in boundary scan, the LDO2 (VDD_SNVS_0V8) goes to 0.95V. In normal condition when then BOOT_MODE3_0 is "0010" (boot from emmc) the LDO2 is 0.8V.

Measuring the VDD_SNVS_0V8 when the BOOT_MODE3_0 signals are at "1111", a frequency of ~32kHz over the 0.8V level is noted. On our board, the VDD_SNVS_0V8 signal is connected to the RTC_XTALO, according to item 3.1.4 - IMX8MNIEC.pdf. 

Could this issue be generated with the connection of VDD_SNVS_0V8 with RTC_XTALO?

Is there any solution to this issue?

Regards,

Estiven

0 Kudos
Reply

2,056 Views
nxf56472
NXP Employee
NXP Employee

I just updated this topic with the NXP recommendation.

0 Kudos
Reply

3,188 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Peter,

     JTAG_MOD is not related to BOOT_MODE pins.

Below is that of I.MX8MM EVK and i.MX8MN

pastedImage_1.png

pastedImage_2.png

Handling method of 2 boards is to pull JTAG_MOD pin to LOW.

Here is BOOT_MODE of 2 boards:

pastedImage_3.png

pastedImage_4.png

Both SOM boards use the same Base board:

pastedImage_5.png

I.MX8M Mini : BOOT_MODE0 & BOOT_MODE1,JTAG_nTRST & TEST_MODE pins.

i.MX8M Nano:   BOOT_MODE0/BOOT_MODE1/BOOT_MODE2/BOOT_MODE3, no TEST_MODE & JTAG_nTRST.

[comment]

--TEST_MODE pin: the pin is for CPU's test mode or normal working mode. when CPU works normally, the pin should be pulled down to LOW.

--JTAG_nTRST pin: For JTAG port, the signal is optional. about this, ARM has a detailed description.

See the link, please!
ARM Information Center 

pastedImage_2.png

Then you can find JTAG interface on base board of these 2 boards:

pastedImage_3.png

Hope above information is helpful for you!

Have a nice day!

B.R,

Weidong

0 Kudos
Reply

3,188 Views
peterlischer
Senior Contributor I

Hi weidong.sun

Thank you for the fast reply. Are you sure that the strapping of the TEST_MODE, BOOT_MODE1, and BOOT_MODE0 are irrelevant for going into the IEEE1149.1 compliant JTAG mode on the i.MX 8M Mini? We have our own i.MX 8M Mini based computer module. The TEST_MODE, BOOT_MODE1, and BOOT_MODE0 are all set to 0 since this is what we need for the final product to boot correctly. However, in production testing, we need to be able to use boundary-scan. As with other i.MX based products, we just set the JTAG_MOD to 0 for going into this mode. Unfortunately, we faced an issue as the read back JTAG ID is wrong. In order to fix that, we need to set the TEST_MODE, BOOT_MODE1, and BOOT_MODE0 to 1. This is quite ugly since we need now a circuit that allows us to change the level of the TEST_MODE, BOOT_MODE1, and BOOT_MODE0 only during production testing. 

I was creating this ticket since I was wondering whether the same issue exists also for the i.MX 8M Nano. I need to know whether we need to add also a circuit on these products in order to use the boundary scan mode during production testing. 

0 Kudos
Reply

2,883 Views
bill_tucker
Contributor II

All

I can get the boundary scan mode to work on the Nano by pulling BOOT_MODE3_0 to "1111" via 4.7k resistors and JTAG_Mod to "0"

 

However, the LDO2 of the BD71847 (VDD_SNVS_0V8) goes to 0.95V from 0.8V when this is done. 

Anybody else observe that?

 

If I don't pull BOOT_MODE3_0 to all 1s, the LDO2 voltage is normal.

 

Bill Tucker

 

 

0 Kudos
Reply

2,459 Views
estiven
Contributor I

Hi @weidong_sun,

I have the same issue as the bill_tucker. When i pulling the BOOT_MODE3_0 signals to "1111" to enter in boundary scan, the LDO2 (VDD_SNVS_0V8) goes to 0.95V. In normal condition when then BOOT_MODE3_0 is "0010" (boot from emmc) the LDO2 is 0.8V.

Measuring the VDD_SNVS_0V8 when the BOOT_MODE3_0 signals are at "1111", a frequency of ~32kHz over the 0.8V level is noted. On our board, the VDD_SNVS_0V8 signal is connected to the RTC_XTALO, according to item 3.1.4 - IMX8MNIEC.pdf. 

Could this issue be generated with the connection of VDD_SNVS_0V8 with RTC_XTALO?

Is there any solution to this issue?

Regards,

Estiven

0 Kudos
Reply

3,188 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Pert,

i.MX Expert gave us feedback, I will send it to you by personal email.

check your email, please!

Weidong

0 Kudos
Reply

3,188 Views
weidong_sun
NXP TechSupport
NXP TechSupport

OK, Peter, I will submit your question to i.mx expert team.

Ask for expert's help.

Wait for my feedback, please!

Have a nice day!

B.R

Weidong

0 Kudos
Reply