JTAG Headers on iMX6 SABRE and QWKS Ref Boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Headers on iMX6 SABRE and QWKS Ref Boards

Jump to solution
1,060 Views
stephenbarton
Contributor II

I have a SABRE MCMiMX6Q Smart Device Board.  It has a 20-pin JTAG Header J6

The schematic for the QWKS-SCMiMX6DQ Ref Board shows a 10-pin JTAG Header J3.

Can anyone tell me which Debuggers will plug directly into these two headers?

Or, do I have to construct my own compatible cable?

Labels (3)
0 Kudos
1 Solution
800 Views
Yuri
NXP Employee
NXP Employee

Hello

  You may look at the following Summary Page :

 

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP 

 

  In particular, ARM DSTREAM with DS-5 and Lauterbach Trace 32 and provbes

may be considered.

 

DSTREAM – ARM Developer 

 

TRACE32® Debugger Hardware 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos
2 Replies
801 Views
Yuri
NXP Employee
NXP Employee

Hello

  You may look at the following Summary Page :

 

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP 

 

  In particular, ARM DSTREAM with DS-5 and Lauterbach Trace 32 and provbes

may be considered.

 

DSTREAM – ARM Developer 

 

TRACE32® Debugger Hardware 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
800 Views
stephenbarton
Contributor II

Thanks you, Yuri, this info is most helpful

0 Kudos