JTAG Flasher, Standalone, with 256MB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Flasher, Standalone, with 256MB

Jump to solution
1,174 Views
waynee
Contributor I

Can anyone recommend a standalone JTAG device that contains 256MB of memory?  I wish to use it on our iMX515 based custom board.  Freescale recommends the Segger Flasher ARM but it only supports 64MB.  We need this feature to load our Linux image for a customer demo.  Thanks for the help.

Wayne

Labels (1)
0 Kudos
1 Solution
1,073 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
4 Replies
1,074 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,073 Views
YixingKong
Senior Contributor IV

Wayne

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
1,073 Views
YixingKong
Senior Contributor IV

Wayne

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
1,073 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,Wayne,

    Yes, exactly, Segger Flasher ARM only supports 64MB, It is not in coincidence with your requirement.

>>Can anyone recommend a standalone JTAG device that contains 256MB of memory?

    You can go to ARM website and evaluate Realvie ICE + RVDS4.x .

Regards,

Weidong

0 Kudos