JB4.3_1.1.0 HDMI output not correct

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JB4.3_1.1.0 HDMI output not correct

1,278 Views
Danube
Contributor IV

Hi Sir,

 

We are testing FSL JB4.3_1.1.0 in MCIMX6QSDP. (B3 version)

 

When we enable LVDS + HDMI function , HDMI output not correct.

My Uboot setting.

setenv bootargs 'console=ttymxc0,115200 androidboot.console=ttymxc0 init=/init rw video=mxcfb0:dev=ldb,LDB-XGA if=RGB666 bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60 fbmem=15M,28M vmalloc=400M fb0base=0x27b00000 enable_wait_mode=off androidboot.hardware=freescale ldo_active=on'

 

 

We also check EDID function and it is correct to detect 1080p TV.

 

 

 

LVDS Panel

8959_8959.jpg_MG_1434.jpg

 

HDMI Site

 

8990_8990.jpg_MG_1432.jpg

Original Attachment has been moved to: JB433_110_error.txt.zip

0 Kudos
Reply
6 Replies

597 Views
Xavier
Contributor III

I'm currently facing the exact same problem and I can't find any piece of answer.

I'm using a RIoTboard with a Farnell LCD8000-70T-EX1 screen connected to the expansion port and a Iiyama ProLite B2280HS screen connected to the HDMI port. I'm running KitKat.

Does anyone have a suggestion?

0 Kudos
Reply

597 Views
EricNelson
Senior Contributor II

Hi Apollo,

I think you need the 'bpp=32' and 'if=RGB24' clauses in the HDMI setup on the kernel command-line.

i.e.

      video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32

0 Kudos
Reply

597 Views
Danube
Contributor IV

Hi Eric,

It is the same issue in HDMI display.

IMAG0600.jpg

0 Kudos
Reply

597 Views
YixingKong
Senior Contributor IV

Apollo

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

597 Views
YixingKong
Senior Contributor IV

Apollo

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos
Reply

597 Views
EricNelson
Senior Contributor II

Well, it was worth a shot...

Do you get the same result if you swap fb0 and fb1?

There are also some configuration files in /system/etc/display_mode_fb0.conf (and fb2 and fb4), but the stock values have always worked for us.

The other thing that you might want to look at are the entries in /sys/class/graphics/fb0/ (and fb2/) to see how things are configured (esp. mode, modes, bits_per_pixel entries)

0 Kudos
Reply