J-LINK can not connect Imx8qxp-CM4 through JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J-LINK can not connect Imx8qxp-CM4 through JTAG

1,368 Views
mengzhu0047
Contributor I

hello,all

I want debug imx8qxp-cm4 using J-link ,but J-link can not find the device.

i am sure the SEGGER patch is installed(iar_segger_support_patch_imx8qx.zip).

i run J-link commander(use JTAG) ,the result is:

pastedImage_1.png

when i use cJTAG,the result is:

pastedImage_2.png

i measure the TDO pin without connecting anything ,it is 0.8V .when connect J-Link, it is 0V.

0 Kudos
Reply
3 Replies

1,085 Views
igorpadykov
NXP Employee
NXP Employee

Hi meng

seems it is required authenticated FW to allow the debug (SCFW loaded first to enable debug).
From attached sect.5.1.3 "Run an example application" Getting Started with MCUXpresso SDK for
i.MX 8QuadXPlus.pdf (included in SDK_2.5.0_MEK-MIMX8QX), pay attention to:

"Make a bootable SD card with the SCFW (System Controller Firmware) image.
See Section 6.3, "Make a bootable SD card with System Controller Firmware (SCFW)""

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,085 Views
mengzhu0047
Contributor I

hi,igorpadykov

Thank you for your reply,I tried the method you mentioned.but it does not work.

i build SCFW use " imx-scfw-porting-kit-1.0.tar.gz"(make qx B=mek R=B0),

but it does not work too.The results are the same as before.

0 Kudos
Reply

1,085 Views
mengzhu0047
Contributor I

what's more,the Imx8qxp does not has A53,but I find the j-link script has this:

pastedImage_1.png

0 Kudos
Reply