It takes about one hour to populate SDK for imx-image-full from imx-5.15.71-2.2.0.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

It takes about one hour to populate SDK for imx-image-full from imx-5.15.71-2.2.0.

Jump to solution
812 Views
MorrisYao
Contributor I

It takes about one hour to populate SDK for imx-image-full from imx-5.15.71-2.2.0. and final SDK is about 26 GB after installing.

Is it possible to remove something to speed it up and shrink the size down?

 

0 Kudos
Reply
1 Solution
797 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it takes sometimes more time to get the image and the space you can build the imx.multimedia image or the core-image and you will save a lot of space, but if you need any gpu or VPU stuff you have to build the full-image.

Regards

 

View solution in original post

0 Kudos
Reply
1 Reply
798 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it takes sometimes more time to get the image and the space you can build the imx.multimedia image or the core-image and you will save a lot of space, but if you need any gpu or VPU stuff you have to build the full-image.

Regards

 

0 Kudos
Reply