It takes about one hour to populate SDK for imx-image-full from imx-5.15.71-2.2.0.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

It takes about one hour to populate SDK for imx-image-full from imx-5.15.71-2.2.0.

跳至解决方案
809 次查看
MorrisYao
Contributor I

It takes about one hour to populate SDK for imx-image-full from imx-5.15.71-2.2.0. and final SDK is about 26 GB after installing.

Is it possible to remove something to speed it up and shrink the size down?

 

0 项奖励
回复
1 解答
794 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it takes sometimes more time to get the image and the space you can build the imx.multimedia image or the core-image and you will save a lot of space, but if you need any gpu or VPU stuff you have to build the full-image.

Regards

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
795 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it takes sometimes more time to get the image and the space you can build the imx.multimedia image or the core-image and you will save a lot of space, but if you need any gpu or VPU stuff you have to build the full-image.

Regards

 

0 项奖励
回复