It's possible Forward traffic from wlan0 to eth0 interface ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

It's possible Forward traffic from wlan0 to eth0 interface ?

1,500 Views
aviau
Contributor II

I'm looking for a solution so that I can stay connected to the wi-fi network and somehow receive data for my application via the eth0 interface, so it doesn't matter if I have SOM's wi-fi enabled or not, because the data from eth0 never stops.

0 Kudos
Reply
2 Replies

1,462 Views
aviau
Contributor II

hello josehp,

thank you for your willingness to help.

In my problem, I need to be connected at the same time to two interfaces, wireless where I will have internet access, and wired where I will have access to a camera, ethernet.

The problem is occurring when I enable wifi, I understand the android framework, but I see that I have no way of maintaining the routing of ip's to allocate the data when I am connected to both.

0 Kudos
Reply

1,479 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

You could try to get connman package in your build.

Regards

0 Kudos
Reply