It's possible Forward traffic from wlan0 to eth0 interface ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

It's possible Forward traffic from wlan0 to eth0 interface ?

1,476 次查看
aviau
Contributor II

I'm looking for a solution so that I can stay connected to the wi-fi network and somehow receive data for my application via the eth0 interface, so it doesn't matter if I have SOM's wi-fi enabled or not, because the data from eth0 never stops.

标记 (5)
0 项奖励
回复
2 回复数

1,438 次查看
aviau
Contributor II

hello josehp,

thank you for your willingness to help.

In my problem, I need to be connected at the same time to two interfaces, wireless where I will have internet access, and wired where I will have access to a camera, ethernet.

The problem is occurring when I enable wifi, I understand the android framework, but I see that I have no way of maintaining the routing of ip's to allocate the data when I am connected to both.

0 项奖励
回复

1,455 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

You could try to get connman package in your build.

Regards

0 项奖励
回复