Does the default BSP code provide a setting of clocks to LAN1 and LAN2 MDC at the same time? Or provide two setting of clocks to MDC1/MDC2 separately?
--->yes,default BSP code provide two MDC, they are two different pad.
pinctrl_eqos: eqosgrp {
fsl,pins = <
MX8MP_IOMUXC_ENET_MDC__ENET_QOS_MDC 0x3
MX8MP_IOMUXC_ENET_MDIO__ENET_QOS_MDIO 0x3
MX8MP_IOMUXC_ENET_RD0__ENET_QOS_RGMII_RD0 0x91
MX8MP_IOMUXC_ENET_RD1__ENET_QOS_RGMII_RD1 0x91
MX8MP_IOMUXC_ENET_RD2__ENET_QOS_RGMII_RD2 0x91
MX8MP_IOMUXC_ENET_RD3__ENET_QOS_RGMII_RD3 0x91
MX8MP_IOMUXC_ENET_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK 0x91
MX8MP_IOMUXC_ENET_RX_CTL__ENET_QOS_RGMII_RX_CTL 0x91
MX8MP_IOMUXC_ENET_TD0__ENET_QOS_RGMII_TD0 0x1f
MX8MP_IOMUXC_ENET_TD1__ENET_QOS_RGMII_TD1 0x1f
MX8MP_IOMUXC_ENET_TD2__ENET_QOS_RGMII_TD2 0x1f
MX8MP_IOMUXC_ENET_TD3__ENET_QOS_RGMII_TD3 0x1f
MX8MP_IOMUXC_ENET_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x1f
MX8MP_IOMUXC_ENET_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK 0x1f
MX8MP_IOMUXC_SAI2_RXC__GPIO4_IO22 0x19
>;
};
pinctrl_fec: fecgrp {
fsl,pins = <
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x3
MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO 0x3
MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0 0x91
MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1 0x91
MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x91
MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x91
MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x91
MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x91
MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0 0x1f
MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1 0x1f
MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x1f
MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x1f
MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x1f
MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x1f
MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02 0x19
>;
};