Issues with serial on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with serial on iMX6

818 Views
bogdananton
Contributor I

Hello we use iMX6DP4AVT1AA  devices in a hardware setup running on windows7 32bit and libusbx-1.0.15-win 

We face some problems on the serial hardware, where we have a FTDI232RL + 3.3V level translation  to comunicate with the iMX chip  .

Sometimes the test system fails when waiting  for  iMX boot console response. 

Is there any hardware alternative to ftdi232rl chip for comunication with imx?

We tryied a alternative using the native COM1  via a max232 + optical isolation and level translation, but the results where worst 

Any sugestions?

Thank you

0 Kudos
Reply
1 Reply

771 Views
igorpadykov
NXP Employee
NXP Employee

Hi bogdan

from i.MX6 side there are no restrictions, one can use any rs232

converter or USB to serial UART interface.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply