Issues with RevC silicon imx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with RevC silicon imx8qxp

2,086 Views
anantha_r
Contributor II

Hi All,

We are facing a strange issue with our device where we use i.mx8x revC silicon.

With the same schematics the device was booting without any issue etc when we were using the RevB version of the silicon but with this new RevC silicon we are facing few issues with booting up a RevC Silicon.

The issue we see is that some time device takes minutes to start booting the bootloader itself. Is there any known issues with revC silicon version? We went through the erratta document but didn't find any conclusive evidence

0 Kudos
Reply
5 Replies

2,069 Views
anantha_r
Contributor II

Hi Igor,

Unfortunately I don't have any MEK for C0 silicon as of now. We have set of units that actually boots up and works fine with C0 silicon, but then there few other units that doesn't come up or sometime take too much time to start the bootloader, when probing the SD Signals we see that there is no interference or so as such and both the waveforms looks same.

FYI, I am using SCFW 1.3.2 , SECO 2.5.4, BSP 2.3.0

0 Kudos
Reply

2,065 Views
igorpadykov
NXP Employee
NXP Employee

Hi anantha_r

 

I am not aware of "BSP 2.3.0", please try latest Linux 5.4.24_2.1.0​ release

described on :

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Use software components (like SECO, SCFW) versions exactly as described in i.MX Linux Release Notes

and rebuild all image from scratch. Do not mix  any "B0" software with "C0".

 

Best regards
igor

0 Kudos
Reply

2,058 Views
anantha_r
Contributor II

Hi igor,

Pardon me for not providing full info

We are using Android 9 with Uboot at L4.14.98.2.0.0 with patches for the C0 silicon revision from this following doc

https://www.nxp.com/docs/en/application-note/AN12770.pdf

 

So I think I don't need to be using the 5.4.1 or so as per this document. If not, please update the document as it might be providing a wrong information to the users

 

0 Kudos
Reply

2,050 Views
igorpadykov
NXP Employee
NXP Employee

Hi anantha_r

 

suggest to try latest android releases:

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Best regards
igor

0 Kudos
Reply

2,076 Views
igorpadykov
NXP Employee
NXP Employee

Hi anantha_r

 

I am not aware of such issues with new silicon, could you try latest

Demo Image with i.MX8QXP MEK board : 

i.MX 8QuadXPlus(C0) MEK

 

Best regards
igor

0 Kudos
Reply