Issue with firmware flashing on i.MX6UL using MfgTool2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with firmware flashing on i.MX6UL using MfgTool2

3,479件の閲覧回数
anupam_mazumdha
Contributor I

I am trying to flash the firmware on Digi ConnectCore 6UL board which is based on NXP i.MX6UL. Steps that I followed:

1) Edited ucl2.xml (attached) as per my board.

2) Edited cfg.ini file (attached)

3) Created sabreauto_files and sabreauto_firmware directory under Profiles\Linux\OS Firmware

4) Copied firmware files into the sabreauto_files directory.

5) Copied mfg tools Linux images into the sabreauto_firmware directory.

6) Set DIP switches on the board.

6) Ran MfgTool2 tool and started it. Here it got stuck and never completed the operation.

Could anyone please tell me what I am doing wrong here?

Thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
10 返答(返信)

3,294件の閲覧回数
anupam_mazumdha
Contributor I

Hi Igor

I was able to load the firmware images using MfgToo2 to RAM and boot u-boot. Could you please help in flashing the firmware images from u-boot prompt like which command to use and on which address to load?

0 件の賞賛
返信

3,280件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>Could you please help in flashing the firmware images from u-boot prompt like which command to use and on which address to load?

 

sorry, could you clarify.  When using mfg tool no need to manually flash

from u-boot prompt. Mfg Tool is doing all automatically.

 

Best regards
igor

 

 

0 件の賞賛
返信

3,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anupam

for using mfg tool it is not necessary to change files, just run

necessary *.vbs script, for example for emmc programming run

mfgtool2-yocto-mx-evk-emmc.vbs

Also for new board (or processor), recommended to run ddr test

and update Mfg Tool firmware (as it was built for i.MX6UL EVK)

as described on

Imx6ull buildroot flash with mfgtool 

Other useful links:

How to build MFG Firmware for i.MX6Q 

AMF-AUT-T2324 - Manufacturing Tool 

https://community.nxp.com/docs/DOC-236994 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,306件の閲覧回数
anupam_mazumdha
Contributor I

Thanks igor for your response. I am trying to program and using otg. Is there any separate step I need to follow?

Thanks

Anupam

0 件の賞賛
返信

3,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anupam

please look at

How-To use NAND boot on i.MX6UL EVK board 

Best regards
igor

0 件の賞賛
返信

3,306件の閲覧回数
anupam_mazumdha
Contributor I

Hi Igor

I do not have EVK board. Can I still use the same vbs script for my ConnectCore i.MX6UL board or shall I use mfgtool2-yocto-mx-14x14-arm2-nand.vbs script?

Thanks

Anupam

0 件の賞賛
返信

3,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anupam

 

I think vbs script can be used, however mfg tool firmware was built for

EVK, so ConnectCore can hang without rebuilding for that particular board.

Some people used it for own boards :

4.4. Installing a Development Build using USB — Working with the Rigado Vesta Gateway v1.0.16 docume... 

 

Best regards
igor

0 件の賞賛
返信

3,306件の閲覧回数
anupam_mazumdha
Contributor I

Thanks Igor. I went through the document on how to rebuild Mfg tool firmware. https://community.nxp.com/servlet/JiveServlet/download/399188-1-274211/How+to+rebuild+MfgTools+firmw... 

But did not understand where should I get the code for it.

Thanks

Anupam

0 件の賞賛
返信

3,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

it is descrbed in sect. 6.2 Manufacturing Tool, MFGTool

Yocto Guide included in  Documentation

Best regards
igor

0 件の賞賛
返信

3,306件の閲覧回数
anupam_mazumdha
Contributor I

Thanks igor for your response. I am trying to flash the nand using OTG cable. Is there any separate step that I need to follow?

Thanks

Anupam

0 件の賞賛
返信