Hello, I am currently deploying a system using the SB-UCM-iMX93-Compulab development board. My project uses a custom camera (Onsemi-AR2020, 20MP, 5120×3840) with output format SBGGR RAW10. The custom camera has its own clock, and does not require a reset or power-up trigger.
- I am using Yocto-project to build a kernel module, which I forked from here:https://github.com/compulab-yokneam/meta-bsp-imx9/blob/EVAL-UCM-iMX93-3.0/README.md
- Previously, I used my camera on the RPi CM4. I then brought up the AR2020 on the i.MX93 after applying some fixes mentioned here:https://www.virtanatech.com/blog/indoor-nano-drones-integrating-a-vio-capable-mipi-csi2-camera-on-th... - And then, I modified Yocto-project with some patches, referencing here:https://github.com/pleiades-br/meta-pleiades-canopus/tree/b58e3fcd92d0b502d0212208bc67da189b57243f/r... With my setup, I started the MIPI camera clock at a relatively low frequency to check whether it must be running. The value was-op_sys_clk_freq_mhz(MIPI_DATA_RATE): 149.4643 MHz. However, it hung during image capture:
root:~# v4l2-ctl --device=/dev/video0 --list-formats-ext
ioctl: VIDIOC_ENUM_FMT
Type: Video Capture Multiplanar
[0]: 'RGBP' (16-bit RGB 5-6-5)
[1]: 'RGB3' (24-bit RGB 8-8-8)
[2]: 'BGR3' (24-bit BGR 8-8-8)
[3]: 'YUYV' (YUYV 4:2:2)
[4]: 'YUV4' (32-bit A/XYUV 8-8-8-8)
[5]: 'NV12' (Y/UV 4:2:0)
[6]: 'NM12' (Y/UV 4:2:0 (N-C))
[7]: 'YM24' (Planar YUV 4:4:4 (N-C))
[8]: 'XR24' (32-bit BGRX 8-8-8-8)
[9]: 'AR24' (32-bit BGRA 8-8-8-8)
[10]: 'BG10' (10-bit Bayer BGBG/GRGR)
Size: Discrete 5120x3840
root:~# v4l2-ctl --device=/dev/video0 --set-fmt-video=width=5120,height=3840,pixelformat=BG10 && v4l2-ctl --device=/dev/video0 --stream-mmap --stream-count=1 --stream-to=output.raw --verbose
VIDIOC_QUERYCAP: ok
VIDIOC_REQBUFS returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_G_FMT returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_STREAMON returned 0 (Success)
^C
--> So I had to cancel at this point.Absolutely no data was captured.:
root:~# ls -l
total 0
-rw-r--r-- 1 root root 0 Feb 27 17:34 output.rawAnd here is the log when I enable it:
Spoiler (Highlight to read) [ 3879.356978] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.357152] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_fmt_mplane
[ 3879.357165] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357173] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357179] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357185] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357191] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357197] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357203] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357209] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357215] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357220] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357226] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357235] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_s_fmt_mplane, fmt=0x30314742
[ 3879.357241] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_fmt_try
[ 3879.357265] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.357271] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.371654] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.371839] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.371850] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.372009] isi-capture 4ae40000.isi:cap_device: cap_vb2_queue_setup, buf_n=4, size=31457280
[ 3879.415864] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_fmt_mplane
[ 3879.415900] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415914] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415921] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415929] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415936] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_fmt_mplane
[ 3879.415945] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_streamon
[ 3879.415957] ar2020 2-0036: ar2020 Calling PowerOn - Kernel Module [1.0.9b]
[ 3879.424109] ar2020 2-0036: ar2020 Done PowerOnStep Without ERROR
[ 3879.433402] mxc-mipi-csi2.0: format: 0x3007
[ 3879.438423] /drivers/staging/media/imx/imx8-isi-hw.c, mxc_isi_channel_set_csc, 361 is using V4L2_PIX_FMT_SBGGR10
[ 3879.438433] bypass csc
[ 3879.438435] input fmt BG10
[ 3879.438438] output fmt BG10
[ 3879.438446] mxc-isi_v1 4ae40000.isi: input_size(5120,3840), output_size(4096,3840)
[ 3879.438465] isi-capture 4ae40000.isi:cap_device: cap_vb2_start_streaming
[ 3879.448967] isi-capture 4ae40000.isi:cap_device: cap_vb2_start_streaming: num_plane=0 discard_size=31457280 discard_buffer=00000000a3278a9c
[ 3879.449013] ar2020 2-0036: Starting stream
[ 3879.548107] ar2020 2-0036: CSI_LANE_MODE confirmed as 2-lane (0x01)
[ 3879.565623] ar2020 2-0036: FRAME_COUNT after streaming: 0xff
[ 3879.565641] ar2020 2-0036: Stream started
[ 3879.565649] dwc-mipi-csi2-host 4ae00000.csi: enter enable=1
[ 3879.565878] dwc-mipi-csi2-host 4ae00000.csi: data_type:0x2b, virtual chan: 0
[ 3879.565884] dwc-mipi-csi2-host 4ae00000.csi: hsa_time=0, hbp_time=0, hsd_time=0, hline_time=1280
[ 3879.565891] dwc-mipi-csi2-host 4ae00000.csi: ipi mode: camera, color_mode: color mode 16
[ 3879.565898] dwc-mipi-csi2-host 4ae00000.csi: format: 0x3007, w/h=(5120, 3840)
[ 3879.565906] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 Version: 0x3135302a
[ 3879.565910] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 lanes: 0x1
[ 3879.565915] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 HOST RESETN: 0x1
[ 3879.565919] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT STATUS MAIN: 0x0
[ 3879.565923] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS1: 0x0
[ 3879.565927] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS2: 0x0
[ 3879.565931] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY CFG: 0x0
[ 3879.565935] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY MODE: 0x0
[ 3879.565939] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT STATUS AP MAIN: 0x0
[ 3879.565943] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS VC1: 0x0
[ 3879.565947] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS VC2: 0x0
[ 3879.565951] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY SHUTDOWN: 0x1
[ 3879.565955] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY RESET: 0x1
[ 3879.565959] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY RX STATUS: 0x10000
[ 3879.565963] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY STOP STATUS: 0x0
[ 3879.565967] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY TEST CTRL0: 0x0
[ 3879.565971] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY TEST CTRL1: 0x0
[ 3879.565975] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG PATTERN HIGH: 0x0
[ 3879.565979] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG PATTERN WIDTH: 0x0
[ 3879.565983] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG CONFIG: 0x0
[ 3879.565987] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG ENABLE: 0x0
[ 3879.565991] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG STATUS: 0x0
[ 3879.565995] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI MODE: 0x1010100
[ 3879.565999] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI VCID: 0x0
[ 3879.566003] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI DATA TYPE: 0x2b
[ 3879.566007] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI SOFT RESET: 0x1
[ 3879.566012] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI ADV FEATURE: 0x0
[ 3879.566016] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_PHY_FATAL: 0x3
[ 3879.566020] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_PKT_FATAL: 0x3
[ 3879.566024] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_PHY: 0x3
[ 3879.566028] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_IPI_FATAL: 0x7f
[ 3879.566032] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_BNDRY_FRAME_FATAL: 0x0
[ 3879.566036] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_SEQ_FRAME_FATAL: 0x0
[ 3879.566040] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_DATA_ID: 0x0
[ 3879.566045] dwc-mipi-csi2-host 4ae00000.csi: gasket: CAMERA MUX: 0x10158
[ 3879.566049] dwc-mipi-csi2-host 4ae00000.csi: gasket: CSI REG: 0x2161c
[ 3879.566054] dwc-mipi-csi2-host 4ae00000.csi: gasket: MIPI -> ISI pixel ctrl: 0xe07
[ 3879.566058] dwc-mipi-csi2-host 4ae00000.csi: gasket: MIPI -> ISI pixel cnt: 0x0
[ 3879.566063] dwc-mipi-csi2-host 4ae00000.csi: gasket: MIPI -> ISI line cnt: 0x0
[ 3879.566069] isi-capture 4ae40000.isi:cap_device: mxc_isi.0.capture is no v4l2 subdev
--> (I cancelled it here)
[ 3880.420390] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_streamoff
[ 3880.420412] isi-capture 4ae40000.isi:cap_device: cap_vb2_stop_streaming
[ 3880.423421] ar2020 2-0036: Stream stopped
[ 3880.423444] dwc-mipi-csi2-host 4ae00000.csi: enter enable=0
[ 3880.423605] isi-capture 4ae40000.isi:cap_device: mxc_isi.0.capture is no v4l2 subdev
root:~# media-ctl -p
Media controller API version 6.6.52
Media device information
------------------------
driver mxc-md
model FSL Capture Media Device
serial
bus info platform:42800000.bus:camera
hw revision 0x0
driver version 6.6.52
Device topology
- entity 1: mxc_isi.0 (16 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "mxc-mipi-csi2.0":4 [ENABLED]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Sink
pad5: Sink
pad6: Sink
pad7: Sink
pad8: Sink
pad9: Sink
pad10: Sink
pad11: Sink
pad12: Source
-> "mxc_isi.0.capture":0 [ENABLED]
pad13: Source
pad14: Source
pad15: Sink
- entity 18: mxc_isi.0.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video0
pad0: Sink
<- "mxc_isi.0":12 [ENABLED]
- entity 22: mxc-mipi-csi2.0 (8 pads, 2 links)
type Node subtype V4L flags 0
device node name /dev/v4l-subdev0
pad0: Sink
<- "ar2020 2-0036":0 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
-> "mxc_isi.0":0 [ENABLED]
pad5: Source
pad6: Source
pad7: Source
- entity 31: ar2020 2-0036 (1 pad, 1 link, 0 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev1
pad0: Source
[stream:0 fmt:SBGGR10_1X10/5120x3840 field:none colorspace:raw xfer:none]
-> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE][ 3879.356978] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.357152] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_fmt_mplane
[ 3879.357165] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357173] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357179] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357185] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357191] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357197] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357203] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357209] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357215] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357220] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357226] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_enum_fmt
[ 3879.357235] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_s_fmt_mplane, fmt=0x30314742
[ 3879.357241] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_fmt_try
[ 3879.357265] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.357271] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.371654] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.371839] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.371850] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_selection
[ 3879.372009] isi-capture 4ae40000.isi:cap_device: cap_vb2_queue_setup, buf_n=4, size=31457280
[ 3879.415864] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_fmt_mplane
[ 3879.415900] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415914] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415921] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415929] isi-capture 4ae40000.isi:cap_device: cap_vb2_buffer_prepare
[ 3879.415936] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_g_fmt_mplane
[ 3879.415945] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_streamon
[ 3879.415957] ar2020 2-0036: ar2020 Calling PowerOn - Kernel Module [1.0.9b]
[ 3879.424109] ar2020 2-0036: ar2020 Done PowerOnStep Without ERROR
[ 3879.433402] mxc-mipi-csi2.0: format: 0x3007
[ 3879.438423] /drivers/staging/media/imx/imx8-isi-hw.c, mxc_isi_channel_set_csc, 361 is using V4L2_PIX_FMT_SBGGR10
[ 3879.438433] bypass csc
[ 3879.438435] input fmt BG10
[ 3879.438438] output fmt BG10
[ 3879.438446] mxc-isi_v1 4ae40000.isi: input_size(5120,3840), output_size(4096,3840)
[ 3879.438465] isi-capture 4ae40000.isi:cap_device: cap_vb2_start_streaming
[ 3879.448967] isi-capture 4ae40000.isi:cap_device: cap_vb2_start_streaming: num_plane=0 discard_size=31457280 discard_buffer=00000000a3278a9c
[ 3879.449013] ar2020 2-0036: Starting stream
[ 3879.548107] ar2020 2-0036: CSI_LANE_MODE confirmed as 2-lane (0x01)
[ 3879.565623] ar2020 2-0036: FRAME_COUNT after streaming: 0xff
[ 3879.565641] ar2020 2-0036: Stream started
[ 3879.565649] dwc-mipi-csi2-host 4ae00000.csi: enter enable=1
[ 3879.565878] dwc-mipi-csi2-host 4ae00000.csi: data_type:0x2b, virtual chan: 0
[ 3879.565884] dwc-mipi-csi2-host 4ae00000.csi: hsa_time=0, hbp_time=0, hsd_time=0, hline_time=1280
[ 3879.565891] dwc-mipi-csi2-host 4ae00000.csi: ipi mode: camera, color_mode: color mode 16
[ 3879.565898] dwc-mipi-csi2-host 4ae00000.csi: format: 0x3007, w/h=(5120, 3840)
[ 3879.565906] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 Version: 0x3135302a
[ 3879.565910] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 lanes: 0x1
[ 3879.565915] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 HOST RESETN: 0x1
[ 3879.565919] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT STATUS MAIN: 0x0
[ 3879.565923] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS1: 0x0
[ 3879.565927] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS2: 0x0
[ 3879.565931] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY CFG: 0x0
[ 3879.565935] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY MODE: 0x0
[ 3879.565939] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT STATUS AP MAIN: 0x0
[ 3879.565943] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS VC1: 0x0
[ 3879.565947] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DATA IDS VC2: 0x0
[ 3879.565951] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY SHUTDOWN: 0x1
[ 3879.565955] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY RESET: 0x1
[ 3879.565959] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY RX STATUS: 0x10000
[ 3879.565963] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY STOP STATUS: 0x0
[ 3879.565967] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY TEST CTRL0: 0x0
[ 3879.565971] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 DPHY TEST CTRL1: 0x0
[ 3879.565975] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG PATTERN HIGH: 0x0
[ 3879.565979] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG PATTERN WIDTH: 0x0
[ 3879.565983] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG CONFIG: 0x0
[ 3879.565987] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG ENABLE: 0x0
[ 3879.565991] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 PPI PG STATUS: 0x0
[ 3879.565995] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI MODE: 0x1010100
[ 3879.565999] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI VCID: 0x0
[ 3879.566003] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI DATA TYPE: 0x2b
[ 3879.566007] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI SOFT RESET: 0x1
[ 3879.566012] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 IPI ADV FEATURE: 0x0
[ 3879.566016] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_PHY_FATAL: 0x3
[ 3879.566020] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_PKT_FATAL: 0x3
[ 3879.566024] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_PHY: 0x3
[ 3879.566028] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_IPI_FATAL: 0x7f
[ 3879.566032] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_BNDRY_FRAME_FATAL: 0x0
[ 3879.566036] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_SEQ_FRAME_FATAL: 0x0
[ 3879.566040] dwc-mipi-csi2-host 4ae00000.csi: DWC CSI2 INT_MSK_DATA_ID: 0x0
[ 3879.566045] dwc-mipi-csi2-host 4ae00000.csi: gasket: CAMERA MUX: 0x10158
[ 3879.566049] dwc-mipi-csi2-host 4ae00000.csi: gasket: CSI REG: 0x2161c
[ 3879.566054] dwc-mipi-csi2-host 4ae00000.csi: gasket: MIPI -> ISI pixel ctrl: 0xe07
[ 3879.566058] dwc-mipi-csi2-host 4ae00000.csi: gasket: MIPI -> ISI pixel cnt: 0x0
[ 3879.566063] dwc-mipi-csi2-host 4ae00000.csi: gasket: MIPI -> ISI line cnt: 0x0
[ 3879.566069] isi-capture 4ae40000.isi:cap_device: mxc_isi.0.capture is no v4l2 subdev
--> (I cancelled it here)
[ 3880.420390] isi-capture 4ae40000.isi:cap_device: mxc_isi_cap_streamoff
[ 3880.420412] isi-capture 4ae40000.isi:cap_device: cap_vb2_stop_streaming
[ 3880.423421] ar2020 2-0036: Stream stopped
[ 3880.423444] dwc-mipi-csi2-host 4ae00000.csi: enter enable=0
[ 3880.423605] isi-capture 4ae40000.isi:cap_device: mxc_isi.0.capture is no v4l2 subdev
root:~# media-ctl -p
Media controller API version 6.6.52
Media device information
------------------------
driver mxc-md
model FSL Capture Media Device
serial
bus info platform:42800000.bus:camera
hw revision 0x0
driver version 6.6.52
Device topology
- entity 1: mxc_isi.0 (16 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "mxc-mipi-csi2.0":4 [ENABLED]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Sink
pad5: Sink
pad6: Sink
pad7: Sink
pad8: Sink
pad9: Sink
pad10: Sink
pad11: Sink
pad12: Source
-> "mxc_isi.0.capture":0 [ENABLED]
pad13: Source
pad14: Source
pad15: Sink
- entity 18: mxc_isi.0.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video0
pad0: Sink
<- "mxc_isi.0":12 [ENABLED]
- entity 22: mxc-mipi-csi2.0 (8 pads, 2 links)
type Node subtype V4L flags 0
device node name /dev/v4l-subdev0
pad0: Sink
<- "ar2020 2-0036":0 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
-> "mxc_isi.0":0 [ENABLED]
pad5: Source
pad6: Source
pad7: Source
- entity 31: ar2020 2-0036 (1 pad, 1 link, 0 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev1
pad0: Source
[stream:0 fmt:SBGGR10_1X10/5120x3840 field:none colorspace:raw xfer:none]
-> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]
Below is my device-tree:
Spoiler (Highlight to read) &cameradev {
status = "okay";
};
/* I2C3 + AR2020 camera */
&lpi2c3 {
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <400000>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pinctrl_lpi2c3>;
pinctrl-1 = <&pinctrl_lpi2c3>;
status = "okay";
ar2020: mipi@36 {
compatible = "onsemi,ar2020";
reg = <0x36>;
clocks = <&clk IMX93_CLK_MIPI_PHY_CFG>;
clock-names = "xvclk";
clock-frequency = <27000000>;
/* clock source sensor */
mipi_csi;
status = "okay";
port {
ar2020_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi_ep>;
clock-lanes = <0>;
data-lanes = <1 2>;
link-frequencies = /bits/ 64 <1500000000>;
clock-noncontinuous;
};
};
};
};
&isi_0 {
status = "okay";
cap_device {
status = "okay";
};
};
/* MIPI CSI interface */
&mipi_csi {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
port@0 {
reg = <0>;
mipi_csi_ep: endpoint {
remote-endpoint = <&ar2020_mipi_ep>;
data-lanes = <2>;
cfg-clk-range = <28>;
hs-clk-range = <0x16>;
bus-type = <4>;
clock-noncontinuous;
};
};
};&cameradev {
status = "okay";
};
/* I2C3 + AR2020 camera */
&lpi2c3 {
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <400000>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pinctrl_lpi2c3>;
pinctrl-1 = <&pinctrl_lpi2c3>;
status = "okay";
ar2020: mipi@36 {
compatible = "onsemi,ar2020";
reg = <0x36>;
clocks = <&clk IMX93_CLK_MIPI_PHY_CFG>;
clock-names = "xvclk";
clock-frequency = <27000000>;
/* clock source sensor */
mipi_csi;
status = "okay";
port {
ar2020_mipi_ep: endpoint {
remote-endpoint = <&mipi_csi_ep>;
clock-lanes = <0>;
data-lanes = <1 2>;
link-frequencies = /bits/ 64 <1500000000>;
clock-noncontinuous;
};
};
};
};
&isi_0 {
status = "okay";
cap_device {
status = "okay";
};
};
/* MIPI CSI interface */
&mipi_csi {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
port@0 {
reg = <0>;
mipi_csi_ep: endpoint {
remote-endpoint = <&ar2020_mipi_ep>;
data-lanes = <2>;
cfg-clk-range = <28>;
hs-clk-range = <0x16>;
bus-type = <4>;
clock-noncontinuous;
};
};
};
Any solution for this, or what can I do now to fix this issue? I attached some Yocto-patches related to the project. I would greatly appreciate any support or suggestions from you. Sincerely, thank you everyone.