Issue with GKI Fragment Modules Not Loading After OTA Update on i.MX8MQ (Android 14_2.0.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with GKI Fragment Modules Not Loading After OTA Update on i.MX8MQ (Android 14_2.0.0)

295 次查看
NaikMK
Contributor I

Dear Team,

We are working with Android 14_2.0.0 on a custom board based on the i.MX8MQ platform. We are including our drivers and kernel modules using a gki.fragment configuration.

Issue Description:
Before OTA Update:

The board boots from the boot_a slot.

All drivers and kernel modules defined in gki.fragment are correctly loaded at boot.

Functionality dependent on these modules works as expected.

After OTA Update:

The board boots successfully from the boot_b slot.

However, none of the drivers or kernel modules from gki.fragment are loaded.

This causes critical features relying on those modules to break.

Additional Information:

  • GKI Kernel Version: 6.6.30
  • Kernel Version Before OTA: 6.6.30-4k-g83331275a61f-dirty
  • Kernel Version After OTA: 6.6.30-android15-8-g63f82df87330-ab12046046-4k

Could you please help us identify what might be missing or misconfigured? We need a solution to ensure that the gki.fragment modules load correctly after an OTA update.

Regards,
Maruti Naik

标签 (1)
0 项奖励
回复
0 回复数