I'm having trouble using the MfgTool to load Linux on an sdCard on an iMX8 EVK. I'm using a Windows 10 host. I have both USB ports connected to the host. I open the file mfgtool2-yocto-mx8-arm2-lpddr4-sdcard-sd2.vbs to launch the manufacturing tool. When I press start, the tool locks up and shows
解決済! 解決策の投稿を見る。
Hello,
Do You have proper Windows 10 driver for UART - USB convertor to run terminal ?
Use the following demo image:
https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8MQ&appType=license
(fsl-image-validation-imx-imx8mqevk.sdcard)
Summary page:
Regards,
Yuri.
Hello,
Which imx 8 are you trying to flash?
And which BSP are you using?
Regards,
Aldo.
iMX8MQ that is on this i.MX 8M Evaluation Kit | NXP EVK.
I'm trying to flash fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard on to a bootable sdcard.
Hi,
For latest releases we suggest to use latest MfgTool-UUU, you can download it form here:
UUU 1.2.135 binary (uuu.exe is for Windows and uuu is for Linux host pc)
Execute the tool in terminal (Linux) or PowerShell as administrator (Windows) with the following command:
Windows:
.\uuu.exe -b sd_all <bootloader>.bin <rootfs>.sdcard
Linux:
$ sudo uuu -b sd_all <bootloader>.bin <rootfs>.sdcard
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I see
e:\Downloads\L4.9.88_2.0.0_images_MX8MQ>c:\Apps\nxp\uuu.exe -b sd_all imx-boot-imx8mqevk-sd.bin-flash_evk fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.135-0-gacaf035
Success 0 Failure 0
1:1 1/ 1 [=================100%=================] SDP: boot -f imx-boot-imx8mqevk-sd.bin-flash_evk
and then nothing else happens. Is that expected?
Hello,
since .sdcard file is just image of SD it is possible to write this image on a host, using Linux dd command
or Win32DiskImager utility under Windows.
Regards,
Yuri.
I have tried writing to the sdcard using the Linux dd command and the EVK did not boot. I have tried writing to the sdcard using balenaEtcher from Windows and the EVK did not boot. I'm using a 32 GB sdcard. That should work, correct?
Hi Yuri,
Thank you for responding. I have boot switches set to
Booting from SD on i.MX 8MQuad EVK
==================================
SWitch D1 D2 D3 D4
SW801 : 1 1 0 0
SW802 : 1 0 (Internal boot mode)
Hello,
Do You have proper Windows 10 driver for UART - USB convertor to run terminal ?
Use the following demo image:
https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8MQ&appType=license
(fsl-image-validation-imx-imx8mqevk.sdcard)
Summary page:
Regards,
Yuri.
Yuri, that image worked! I am up and running!
For the record, I just used balenaEtcher to copy the sdcard image to an sdcard and then I plugged the sdcard in to the EVK, made sure the dip switches were set correctly and it booted fine.
Are there default versions of cfg.ini and UICfg.ini that can be used to program the EVK? I'm not clear whether or not I have to edit those files to program an image that comes from NxP on the the EVK?