Issue "cpu cpu0: failed to scale vddarm down" in latest bsp imx-5.4.24-2.1.0.xml

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue "cpu cpu0: failed to scale vddarm down" in latest bsp imx-5.4.24-2.1.0.xml

ソリューションへジャンプ
869件の閲覧回数
rakesh_patel
Senior Contributor I

Kernel logs

==================

[ 2.643832] imx_thermal tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C
[ 2.654567] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 2020-10-05T12:17:28 UTC (1601900248)
[ 2.668050] EXT4-fs (mmcblk3p2): mounting ext3 file system using the ext4 subsystem
[ 2.695910] 996 MHz, 1250 mV --> 396 MHz, 1175 mV
[ 2.700696] SW1AB: Restricting voltage, 1250000-1175000uV
[ 2.706552] SW1AB: Restricting voltage, 1250000-1175000uV
[ 2.712389] cpu cpu0: failed to scale vddarm down: -22
[ 2.718011] SW1AB: Restricting voltage, 1250000-1175000uV
[ 2.723821] SW1AB: Restricting voltage, 1250000-1175000uV
[ 2.729709] cpu cpu0: failed to scale vddsoc down: -22
[ 2.736015] 396 MHz, 1250 mV --> 996 MHz, 1250 mV
[ 2.747484] EXT4-fs (mmcblk3p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.755685] VFS: Mounted root (ext3 filesystem) on device 179:2.
[ 2.761906] 996 MHz, 1250 mV --> 792 MHz, 1175 mV
[ 2.767385] SW1AB: Restricting voltage, 1250000-1175000uV
[ 2.773155] devtmpfs: mounted
[ 2.776192] SW1AB: Restricting voltage, 1250000-1175000uV

 

Dts configuration

===========

operating-points = <
/* kHz uV */
996000 1250000
792000 1175000
396000 1175000
>;
fsl,soc-operating-points = <
/* ARM kHz SOC uV */
996000 1250000
792000 1175000
396000 1175000
>;

 

Issue

========

1) Why failed to scale vddsoc down issue? 

ラベル(1)
0 件の賞賛
返信
1 解決策
862件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rakesh_patel

 

one can try to adjust "operating-points" according to datasheet vlaues, in particular

automotive grade has not "996000" point according to Table 10. Operating Ranges

i.MX 6SoloX Automotive and Infotainment Applications Processors - Data Sheet

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
863件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rakesh_patel

 

one can try to adjust "operating-points" according to datasheet vlaues, in particular

automotive grade has not "996000" point according to Table 10. Operating Ranges

i.MX 6SoloX Automotive and Infotainment Applications Processors - Data Sheet

 

Best regards
igor

0 件の賞賛
返信
848件の閲覧回数
rakesh_patel
Senior Contributor I

Removing 996 freq, works fine.

0 件の賞賛
返信