Issue in swupdate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in swupdate

2,334 Views
sd05
Contributor III

Hello Community,

I am working on yocto upgradation from Warrior to Hardknott. I am facing  an issue when I am trying to do software update using "swupdate -i" command, I am getting following error:

Getting following error:

[ERROR] : SWUPDATE failed [0] ERROR : archive_read_next_header(): Pathname can't be converted from UTF-8 to current locale. 1

[ERROR] : SWUPDATE failed [0] ERROR : copyimage status code is -14

 

I have tried adding following patch but still getting same error

https://github.com/sbabic/swupdate/compare/master...jameshilliard:locale

 

Also please note I am able to update if I use warrior .swu image.

Please answer...thanks!

0 Kudos
Reply
1 Reply

2,323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sunidhi

 

this is specific yocto issue and it can be posted on meta-fsl-arm mailing list

https://lists.yoctoproject.org/g/meta-freescale

 

Best regards
igor

0 Kudos
Reply