Hi,
I am trying to run an image on the target but encountered some difficulties in entering the U-Boot prompt.
I first attempted to download the image using MFQTool in SD3 boot mode.
cfg.ini
{LIST}
name=ubuntu-SabreSD-eMMC
After downloading Images using MFQTool, i switch back to eMMC4.4 boot mode.
When i restart the board, I'm not able to see the count down timer for me to enter the U-Boot prompt.
I get the following instead.
UBoot 2009 08 (Apr 25 2013 - 01:17:52)
..
..
..
Board:i.Mx^Q-SABRESD: unknown-board Board:0x63012 [ POR ]
Boot Device: MMC
I2C: ready
DRAM: 1GB
MMC: FSL_USDHC:0, FSL_USDHC:2, FSL_USDHC:3
if anyone has encountered similar situation or has a solution for it, please share it with me. Thanks