Hi,
I am trying to run an image on the target but encountered some difficulties in entering the U-Boot prompt.
I first attempted to download the image using MFQTool in SD3 boot mode.
cfg.ini
{LIST}
name=ubuntu-SabreSD-eMMC
After downloading Images using MFQTool, i switch back to eMMC4.4 boot mode.
When i restart the board, I'm not able to see the count down timer for me to enter the U-Boot prompt.
I get the following instead.
UBoot 2009 08 (Apr 25 2013 - 01:17:52)
..
..
..
Board:i.Mx^Q-SABRESD: unknown-board Board:0x63012 [ POR ]
Boot Device: MMC
I2C: ready
DRAM: 1GB
MMC: FSL_USDHC:0, FSL_USDHC:2, FSL_USDHC:3
if anyone has encountered similar situation or has a solution for it, please share it with me. Thanks
SWI
We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to
reply with an update to this discussion.
Thanks,
Yixing
SWI
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the
issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing