Hi NXP team,
I am trying to mount an USB 1 and USB 2 automatically using "fstab.freescale" file with mount point /mnt/usb1 and /mnt/usb2. Mount point name is not reflecting during mount time which I have changed manually ie Two usb are mounting to a default path called /mnt/media_rw/ instead of /mnt/usb1 and /mnt/usb2 .
Kindly help me to sort out this issue and provide some possible solutions also.
Note: Need to use voldmanaged as fs_mgr_flags which provides hotplug feature for android
USB1: chipidea (HOST)
USB2: cadence ( HOST)
fstab.freescale file:
/devices/platform/bus@5b000000/5b0d0000.usb/ci_hdrc.0/* /mnt/usb1 auto defaults voldmanaged=usb:auto
/devices/platform/bus@5b000000/5b110000.usb3/* /mnt/usb2 auto defaults voldmanaged=usb:auto
解決済! 解決策の投稿を見る。
HI NXP team & community members,
Is the USB mount problem solvable? Waiting for your precious solutions.