Dear Sir or Madam,
Customer's board happened below issue.
[Status]
Device: i.MX6D
BSP: Yocto L3.10.17
Board: Custom board
SSI: I2S Master mode
Output: 4ch data output with network mode as normal bit clock + frame
ideal Frame Rate=44.1kHz
[Issue]
Phenomenon: Sound noize from both of Left and Right
Contents: 4ch Wav file(Left-ch:beep sound, Other 3-ch: No sound)
Detail:
- Refer to attached waveform. It looks LRCLK raise up early for 1ch interval.
- This phenomenon was confirmed on SABRE-SDP with custom setting, too.
[Register setting]
Refer to i.MX 6Dual/6Quad Applications Processor Reference Manual(p.5122) "Table 61-7. SSI Bit Clock and Frame
Rate as a Function of PSR, PM, and DIV2"
SSI's sys clock=11.2896MHz, DIV=0, PSR=0, PW=1, WL=7, DC=3
- SSI
scr=0xbb // TCH_EN = 0
sier=0x1b80f00
stcr=0x2ed // TFEN0 = 1, TFEN1 = 0
srcr=0x2cd // RFEN0 = 1, RFEN1 = 0
stccr=0xe201
srccr=0xe201
sfcsr=0x880688
stmsk=0xfffffff0
srmsk=0xfffffff0
- port1(Internal Port)
ptcr=0x800
pdcr=0xa000
- port6(External Port)
ptcr=0x84010800
pdcr=0x0
[Question]
Q1:
Do you find this cause?
Please give me some advice?
Q2:
Refer to below description.
----------------------------------------------------------------------------------------------------
61.2.1 Signals Overview
SRCK
Serial Receive Clock. SRCK can be used as either an input or an output. This clock signal is used by the receiver
in asynchronous mode and is always continuous. During S, the STCK port is used instead for clocking in data. In
SSI synchronous modes, this port can be used as an output for the network clock (oversampling clock) . In I2S
master mode, this signal can be used to output the network clock to an external CODEC.
----------------------------------------------------------------------------------------------------
I consider that AUD6_RxC(equivalent to SRCK) doesn't have to connect.
Is it right in the following connection?
[Customer's connection]
BCLK(AUD6_TxC)
LRCLK(AUD6_TxFS)
DACDAT(AUD6_TxD)
MCLK(AUD_MCLK)
I attached more detail information.
Please check it, too!
(See attached file: (Detail)Waveform of Audio Codec)
Best Regards,
Keita
Here is a quick workaround I did for getting SSI to work in master mode on imx6q-sabresd running kernel 3.18:
[alsa-devel] No sound captured with SGTL5000 on i.MX6 in I²S master mode
Hi Fabio,
Thank you for your information!
But, my customer had already set your mentioned.
>No sound captured with SGTL ~
Now the MX6Q-SDP output the sound. But it is very noisy.
Best Regards,
Keita
Hi Saurabh,
Thank you for your reply.
Now, my customer is evaluating it on i.MX6Q SABRE-SDP.
>Just make sure that SSI clk and MCLK derived from same clock source.
"MCLK from GPIO_0(CLKO) && BCLK from AUD3_TXC."
BR,
Keita
Hi
Keita
static struct clk clko_clk = {
__INIT_CLK_DEBUG(clko_clk)
//.parent = &pll2_528_bus_main_clk,
.parent = &pll4_audio_main_clk,
.enable = _clk_enable1,
static struct clk ssi1_clk = {
__INIT_CLK_DEBUG(ssi1_clk)
//.parent = &pll3_pfd_508M,
.parent = &pll4_audio_main_clk,
.enable_reg = MXC_CCM_CCGR5,
clk_set_rate(&pll4_audio_main_clk, /*176000000*/ 180633600); | //44100 base rate --> 44100*8*512 =180633600 |
Please check above code, I have modified it for 3.0.35 kernel, You need to make modification according to it.
Thanks
Saurabh