Issue About IMX6S And PMIC PF100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue About IMX6S And PMIC PF100

1,535 Views
tony_l_cai
Contributor III


Hi All,

Could I get the demo schematic of IMX6S, and the startup sequence of PF100F0?

Thank you~

Labels (4)
0 Kudos
Reply
1 Reply

1,202 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tony

one can use attached MCIMX6DL_SDP schematic, full design is located on:

Schematics (1)

Design files, including hardware schematics, Gerbers, and OrCAD files.

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

startup sequence is on Table 10. Start-up Configuration MMPF0100 Datasheet

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply