Is using HAB appropriate to check integrity and to force to use 2nd bootloader if changed?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is using HAB appropriate to check integrity and to force to use 2nd bootloader if changed?

979 次查看
sunghyunahn
Contributor I

Dear all,

I’m implementing “fail safe booting” using redundant boot images.

It aims "booting succesfully" even though there are some damages on booting images.
I made a plan to use HAB feature for some part of functionalities.

i.mx6 dual processor is supposed to be used and AI board is referenced.

I designed configuration and procedures as below to overcome boot fail situation due to damaged boot images.
1. duplicate boot images (1st and 2nd bootloaders and kernels)
2. check validity of 1st bootloader
3. check 2nd bootloader if 1st one is damaged
4. use a valid bootloader to load kernel
5. check validity of 1st kernel
6. check 2nd kernel if 1st one is damaged
7. load a valid kernel
8. after boot;
     A. check validity of 2nd bootloader if booted using 1st bootloader
     B. check validity of 2nd kernel if booted using 1st kernel
     C. recover damaged images, if any, by copying valid corresponding images

Because steps 5~7 are done buy bootloader I can implement it without any dependency.
But steps 2~4 are executed by codes in ROM and it depends on features of i.mx6 dual processor.

By investigating on documents I found that I could use HAB feature to check integrity of bootloader and
to force to use 2nd bootloader if 1st bootloader is changed. (Step 2~4)

References;
IMX6DQRM - i.MX 6Dual_6Quad Applications Processor Reference Manual
i.MX_6_Linux_High_Assurance_Boot_(HAB)_User's_Guide

My questions;
1. Is using HAB appropriate to check validity and to force to use 2nd bootloader if changed?
2. Is it possible to recover (Step. 8) even the device is “closed” - SEC_CONFIG[1] fused?
3. To test HAB function I may need to burn some eFuses and public keys.
     A. I want to avoid fusing reference board because it is irreversible.
          Is there any way to make board operate like fused? (fusing emulation?)
     B. For the production, Do eFuses and public keys need to be burnt during process of production? If then, is there any suggesting or general way?

Thanks.

Sunghyun Ahn

标签 (4)
0 项奖励
回复
1 回复

890 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sunghyun

>1. Is using HAB appropriate to check validity and to force to use 2nd bootloader if changed?

>2. Is it possible to recover (Step. 8) even the device is “closed” - SEC_CONFIG[1] fused?

yes, please check Figure 4-1. Boot Flow i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

> Is there any way to make board operate like fused? (fusing emulation?)

I am afraid not

>B. For the production, Do eFuses and public keys need to be burnt during process

>of production? If then, is there any suggesting or general way?

for fuse programming one can refer to sect.3.3. Fuse programming AN4581 Secure Boot.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复