Is there any way to suspend and wakeup the Bluetooth functionality in IMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any way to suspend and wakeup the Bluetooth functionality in IMX8QM

ソリューションへジャンプ
1,536件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

 

Board: IMX8QM Custom platform

OS: Yocto - L5.10.XX

I am planning to do Suspend and Wakeup the Bluetooth functionality. But, I unable to find in the Bluetooth driver. 

Is there any way, to make Bluetooth Suspend and Wakeup.

 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
1 解決策
1,524件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

seems it could be possible if bluetooth device has some gpio connected to processor.

Gpio can be used for waking processor. Below article may be helpful

https://docs.microsoft.com/en-us/windows-hardware/design/device-experiences/bluetooth-power-manageme...

 

Best regards
igor

元の投稿で解決策を見る

1 返信
1,525件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

seems it could be possible if bluetooth device has some gpio connected to processor.

Gpio can be used for waking processor. Below article may be helpful

https://docs.microsoft.com/en-us/windows-hardware/design/device-experiences/bluetooth-power-manageme...

 

Best regards
igor