Is there any way to suspend and wakeup the Bluetooth functionality in IMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any way to suspend and wakeup the Bluetooth functionality in IMX8QM

跳至解决方案
1,538 次查看
vinothkumars
Senior Contributor IV

Hi All,

 

Board: IMX8QM Custom platform

OS: Yocto - L5.10.XX

I am planning to do Suspend and Wakeup the Bluetooth functionality. But, I unable to find in the Bluetooth driver. 

Is there any way, to make Bluetooth Suspend and Wakeup.

 

 

Regards,
Vinothkumar Sekar
0 项奖励
回复
1 解答
1,526 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

seems it could be possible if bluetooth device has some gpio connected to processor.

Gpio can be used for waking processor. Below article may be helpful

https://docs.microsoft.com/en-us/windows-hardware/design/device-experiences/bluetooth-power-manageme...

 

Best regards
igor

在原帖中查看解决方案

1 回复
1,527 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

seems it could be possible if bluetooth device has some gpio connected to processor.

Gpio can be used for waking processor. Below article may be helpful

https://docs.microsoft.com/en-us/windows-hardware/design/device-experiences/bluetooth-power-manageme...

 

Best regards
igor