Is there any tool or method to make i.max8qm boot.img

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any tool or method to make i.max8qm boot.img

706 Views
zbm030823
Contributor II

Hi ,when i read boot img structure of i.max8qm RM ,i want to make boot img of i.max8qm which can be supported several different oses's imgs such as android img on A53 and linux img on A72.Could any one share me the method or which tool to do this?

0 Kudos
Reply
2 Replies

590 Views
zbm030823
Contributor II

Hi Bio_TICFSL,

Thanks very much!But I would like to use hardware virtualization by SCU of I.max8qm,I foud imx-mkimg can make this boot img structure.For an example, ./$(MKIMG) -soc QM -c -dcd $(DCD_CFG) -scfw scfw_tcm.bin -m4 m4_image.bin 0 0x34FE0000 -csf csf.bin -scd scd.bin -c -ap u-boot-atf.bin a53 0x80000000 -csf csf_ap.bin -out flash.bin.This is only one os supported,if supported two oses such as android and linux, what is a72 entry address?And how to make u-boot-atf.bin for a53 and u-boot-*.bin for a72?

0 Kudos
Reply

590 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Zhu,

The are many methods of virtualization, you can see this presentation for better understanding,

https://community.nxp.com/docs/DOC-330318 

Regards

0 Kudos
Reply