Is there any restrict to copy a data from i.MX6Q PCIe to DDR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any restrict to copy a data from i.MX6Q PCIe to DDR?

Jump to solution
1,141 Views
satoshishimoda
Senior Contributor I

Hi all,

I tried data transfer from FPGA to DDR3 which is connected to i.MX6Q via PCIe I/F as attached file.

However, it was failed with some reason.

Then, I guess this transfer was prevented by i.MX6Q since i.MX6Q don't allow read / write to DDR3 by FPGA via PCIe.

So could you let me know whether there is some setting to allow read / write access from PCIe to DDR3?

And if there is the setting, could you let me know how to change it?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (2)
1 Solution
844 Views
b47504
NXP Employee
NXP Employee

If imx6q worked as Endpoint mode,  we need to configure imx6 Pcie BAR(write your special address to pcie bar register for address match) to support system memory access from root complex, aligned to PCIe spec.

View solution in original post

0 Kudos
Reply
1 Reply
845 Views
b47504
NXP Employee
NXP Employee

If imx6q worked as Endpoint mode,  we need to configure imx6 Pcie BAR(write your special address to pcie bar register for address match) to support system memory access from root complex, aligned to PCIe spec.

0 Kudos
Reply