Is there any problem with video encoder in IMX8qxp?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any problem with video encoder in IMX8qxp?

1,632件の閲覧回数
wasim_nazir
Contributor II

Hi,

Bio_TICFSL‌, igorpadykov sureshrao

I see white lines on display whenever i do screengrab. Also, its visible sometimes when I do video encoding of frames coming from camera.

Is this known issue with imx8qxp(android 9.2.3)

Thanks in Advance,

Wasim 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,539件の閲覧回数
wasim_nazir
Contributor II

Hi igorpadykov‌,

Thanks for your reply.

I can see there are lot of fixes, viz:

      • GPU: Fix OpenCV and Vulkan conformance issues.

      • VPU: Enhancement for encoder and decoder using different reset signal

      • MIPI_DSI: Bug fixes to resolve MIPI DSI CRC issue for LP DCS long write.

But, I am using Rev.B0 and I don't think we can change it as of now.

But is there any chance of getting any fix for the issue I had mentioned above or is the issue fixable in B0?

Thanks

0 件の賞賛
返信

1,539件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wasim

rev.B0 is not recommended for production purposes.

Best regards
igor

0 件の賞賛
返信

1,539件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wasim

rev.C0 improved many features as described in

i.MX 8X C0 Migration Guide Migrating from i.MX 8X B0 to i.MX 8X C0

Please try that revision with Android supporting that part, like Android  P9.0.0_2.3.2

Android P9.0.0_2.3.2 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信