Is there any patch support mpu 8080 LCD on i.mx6sx ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any patch support mpu 8080 LCD on i.mx6sx ?

581件の閲覧回数
allen_kim1
Contributor I

Dear Community

i red that documentation https://community.nxp.com/docs/DOC-331754 

is there any patch support MPU 8080 LCD on i.mx6SX ? 

Thanks BR

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

421件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Allen

I am not aware of such patch but since i.MX6SX has similar eLCDIF,

these should be easily adapted to i.MX6SX. Suggest to elevate request

using local fae channel for specific kernel patch version.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信