Is there any i.MX6 hardware platform good for developing an IP PBX system?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any i.MX6 hardware platform good for developing an IP PBX system?

907 次查看
nguyenanhduc
Contributor I

Hi everyone,

I am in the process of looking for a hardware platform to develop an IP PBX system. It should be pretty powerful due to the required tasks such as VoIP gateways. I am considering i.mx6 due to it impressive capability; however, I can not find any information on the Internet that presents the use of i.mx6 for ip pbx, which makes me feel I am going into wrong directions. Please kindly help me resolve this problem. In case, i.MX6 is not a good choice for my applications, any suggest on other platforms will be greatly appreciated,

With best regards,

Nguyen Anh Duc

标签 (2)
0 项奖励
回复
1 回复

844 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Nguyen,

I have seen customers that have used the i.MX6Q for PBX systems, though unfortunately we do not have an app note or any documentation for you to guide in the development of a PBX system.

Indeed the i.MX6 is a good fit for it, the NEON processor helps a lot.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复