Is there any different firmwares for the VPU with improved codec capabilities?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any different firmwares for the VPU with improved codec capabilities?

跳至解决方案
1,498 次查看
luisaguiar
Contributor I

What i want to know if it is possible to change the VPU firmware for another that has better capabilities. Is there another firmware binary? what changes to linux would be needed to make it work?

标签 (3)
标记 (3)
0 项奖励
回复
1 解答
1,384 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Luis

VPU firmware is included in BSP, its current revision is given

in Release Notes document. VPU capabilities mainly defined

by hardware bus bandwidth and not firmware and can not be significantly changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,385 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Luis

VPU firmware is included in BSP, its current revision is given

in Release Notes document. VPU capabilities mainly defined

by hardware bus bandwidth and not firmware and can not be significantly changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,384 次查看
luisaguiar
Contributor I

Hi igor,

Thanks for your reply.

I was referring mostly to H264 support for Main and High profiles. I already tested the VPU and it works well at Full HD @ 30 fps (level 4.0) but only constrained Base profile.

But, has you explained, it would probably need different hardware that is not available on the VPU module to support the added features.

Best regards,

Luis

0 项奖励
回复