I can find the Linux mfg tool "mfgtoolcli" in the same directory of MfgTool2.exe
With mfgtoolcli, there are linux-ver-usage, linux-runvbs.sh, linux-cvbs.sh
And document mfgtools\Document\Eclipse Plugin and mfgtoolcli\mfgtoolcli-readme
Requirement:
- libusb-1.0-0-dev
- libusb-1.0-0
Usage:
./linux-runvbs.sh <vbs file> to kick off mfgtool for specific platform,
or launch ./linux-cvbs.sh to covert all vbs to bash scripts.
Hi Doug,
unfortunately there is not a version of MFGtool for Linux.
Sorry for the inconvenience.
Carlos
Hi Carlos,
Are you sure?? I'd say otherwise:
GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.
Branch master: linux version
Branch windows: windows version
Note however that it is a command-line version of mfgtools, no UI, but the result is the same.
Regards,
Gary
Hi Gary,
Have you had success in using this version of the tool?
I've compiled it ok (albeit there's lots of warnings!). I think I have suitable ini and xml files, but I can't get beyond the first stage (even running with sudo).
The console just shows
Your Options:
Ready to flash.
1 Done! [================================================>] "Boot" body="Recovery" error, file="./P
With the log file showing
ModuleID[2] LevelID[1]: MxHidDevice::Read() Error reading from device 0x-7 with size 1025.
ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!!
ModuleID[2] LevelID[1]: Failed to initialize memory!
ModuleID[2] LevelID[1]: PortMgrDlg(0)--MxHidDevice--Command Boot excute failed
Hi,
Yes I tried it long time ago (when I pushed some patches to the project) and it worked ok.
Make sure to check your file name, "./P" seems strange.
Regards,
Gary
I think that's just the terminal truncating the file - if I widen it then it shows more of the correct path. (And strace seems to show all the files being opened ok).