Is there a step-by-step sample for set boot mode to boot from fuse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a step-by-step sample for set boot mode to boot from fuse

385件の閲覧回数
13614278
Contributor III

I read the IMX8MINI RM document, in Table6-1, it says if BOOT_MODE[1:0] is 00, that it is Boot from Fuse.

 

So could someone give me a step-by-step sample, to set above BOOT_MDOE[1:0] to 00? Because i am a software engineer, it is difficult for me to understand above statement, should I enter uboot mode to use 'fuse' command to do this? if it is , how to do it? how should I pass the command parameter?

 

Thanks

ラベル(1)
0 件の賞賛
返信
0 返答(返信)