Is there a recommended PMIC for use with the i.MX 6ULL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a recommended PMIC for use with the i.MX 6ULL?

432 次查看
dcade
Contributor I

I see the PF3001 is recommended for use with the 6UL but no mention of the 6ULL?

0 项奖励
回复
1 回复

380 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

6ULL is reduced version of 6UL, so the same pmic can be used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复